Part Number: TMS320F28379D
在使用CCS软件9.0时,由于测试需要cmd文件中.text 和.econst 设置的大小不够用了,于是就更改了2837xD_RAM_lnk_cpu1.cmd文件,文件见插入的代码,然后就出现需要点两次Resume情况,请问有没有遇到类似情况的,该如何解决?
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x000000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
/* RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800*/
RESET : origin = 0x3FFFC0, length = 0x000002
RAMLS1_4 : origin = 0x008800, length = 0x002000
RAMGS6_11 : origin = 0x012000, length = 0x006000
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2 : origin = 0x00E000, length = 0x004000
// RAMGS3 : origin = 0x00F000, length = 0x001000
// RAMGS4 : origin = 0x010000, length = 0x001000
// RAMGS5 : origin = 0x011000, length = 0x001000
/* RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
RAMGS10 : origin = 0x016000, length = 0x001000
RAMGS11 : origin = 0x017000, length = 0x001000*/
RAMGS12_15 : origin = 0x018000, length = 0x004000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
// RAMGS13 : origin = 0x019000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
// RAMGS14 : origin = 0x01A000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
// RAMGS15 : origin = 0x01B000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
CANA_MSG_RAM : origin = 0x049000, length = 0x000800
CANB_MSG_RAM : origin = 0x04B000, length = 0x000800
}
SECTIONS
{
codestart : > BEGIN, PAGE = 0
ramfuncs : > RAMM0 PAGE = 0
// .text : >>RAMM0 | RAMD0 | RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4, PAGE = 0
.text : >> RAMM0 | RAMD0 | RAMLS1_4 | RAMGS6_11, PAGE = 0
.cinit : > RAMM0, PAGE = 0
.pinit : > RAMM0, PAGE = 0
.switch : > RAMM0, PAGE = 0
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.stack : > RAMM1, PAGE = 1
.ebss : > RAMLS5, PAGE = 1
.econst : >> RAMGS2 | RAMGS12_15, PAGE = 1
.esysmem : > RAMLS5, PAGE = 1
Filter_RegsFile : > RAMGS0, PAGE = 1
ramgs0 : > RAMGS0, PAGE = 1
ramgs1 : > RAMGS1, PAGE = 1
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} > RAMM0, PAGE = 0
#else
ramfuncs : > RAMM0 PAGE = 0
#endif
#endif
/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}
GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
/* The following section definition are for SDFM examples
Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444
Difference_RegsFile : >RAMGS5, PAGE = 1, fill=0x3333*/
}