Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: MOTORWARE, C2000WARE
程序路径:A:\TI\motorware_1_01_00_18\sw\solutions\instaspin_motion\boards\boostxldrv8305_revA\f28x\f2806xM\projects\ccs\proj_lab13b
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: MOTORWARE, C2000WARE
程序路径:A:\TI\motorware_1_01_00_18\sw\solutions\instaspin_motion\boards\boostxldrv8305_revA\f28x\f2806xM\projects\ccs\proj_lab13b
请问怎么便利添加相应的SCI中断及其函数应用呢,C2000 ware中是否由相应的手册或例子呢? 不太熟悉TI的生态系统
C2000WARE中有SCI的例程,你可以参考一下例程:C:\ti\c2000\C2000Ware_3_04_00_00\device_support\f2806x\examples\c28\scia_loopback_interrupts
请问上述路径下的scia_loopback和sci_echoback 两个串口通讯例程有什么区别? 光从字面上难以理解什么意思
你可以看一下main函数所在.c文件开头注释中的介绍,里面包含了程序介绍、设置、外部连接、观测口等等很全面的信息。比如Example_2806xSci_Echoback.c中:
//! This test receives and echo-backs data through the SCI-A port. //! //! The PC application 'hypterterminal' can be used to view the data //! from the SCI and to send information to the SCI. Characters received //! by the SCI port are sent back to the host. //! //! \b Running \b the \b Application //! -# Configure hyperterminal: //! Use the included hyperterminal configuration file SCI_96.ht. //! To load this configuration in hyperterminal //! -# Open hyperterminal //! -# Go to file->open //! -# Browse to the location of the project and //! select the SCI_96.ht file. //! -# Check the COM port. //! The configuration file is currently setup for COM1. //! If this is not correct, disconnect (Call->Disconnect) //! Open the File-Properties dialog and select the correct COM port. //! -# Connect hyperterminal Call->Call //! and then start the 2806x SCI echoback program execution. //! -# The program will print out a greeting and then ask you to //! enter a character which it will echo back to hyperterminal. //! //! \note If you are unable to open the .ht file, you can create //! a new one with the following settings //! - Find correct COM port //! - Bits per second = 9600 //! - Date Bits = 8 //! - Parity = None //! - Stop Bits = 1 //! - Hardware Control = None //! //! \b Watch \b Variables \n //! - \b LoopCount, for the number of characters sent //! - ErrorCount //! //! \b External \b Connections \n //! Connect the SCI-A port to a PC via a transceiver and cable. //! - GPIO28 is SCI_A-RXD (Connect to Pin3, PC-TX, of serial DB9 cable) //! - GPIO29 is SCI_A-TXD (Connect to Pin2, PC-RX, of serial DB9 cable)