This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: 配置问题

Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE

1:新的F280049C,第一次下载程序,如果使用SCI下载,只能使用SCIA 的GPIO28和GPIO29引脚吗?

2:F280049C的SDFM模块,使用32的抽取率,输出16位结果,在电流不变的情况下输出结果会在正负64之间跳变,这个跳动正常吗?

  • 1、默认的SCI boot是SCIA。

    2、我认为跳变不太正常。有没有用例程测试过?C:\ti\c2000\C2000Ware_3_04_00_00\driverlib\f28004x\examples\sdfm

  • 1:SDMF的跳动,我使用官方例程在测试一下。

    2:我现在有个新问题,配置了同组中断线中的两个中断PWM1_INT和PWM4_INT,PWM4_INT的优先级高于PWM1_INT。实际工作中PWM1_INT先触发,在PWM1_INT中断服务函数未执行完时,PWM4_INT中断触发,但PWM4_INT中断没有打断PWM1_INT中断。F280049C的同组中断可以嵌套吗?

  • 问题二:F280049的中断默认条件下不支持嵌套,想要完成中断嵌套,需要特殊处理。