This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069F: DSP

Part Number: TMS320F28069F


板子仿真时,出现以下错误·,在查手册时发现,问题可能是JTAG的管脚与地短路,但是测量时,并未短路。之前程序可以下载进去,后来出现了以下问题。那么主要原因可能是什么呢?

Error connecting to the target:
(Error -233 @ 0x0)
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
(Emulation package 9.1.0.00001)