使用XDS110仿真器烧录到Flash,并在线仿真运行,上位机发送数据,SCI能进入中断,并接收到完整的数据。当我拔掉仿真器,通过USB重新上电,重新打开串口,并通过上位机发送数据,DSP无法进入SCI接收中断接收到SCI数据,但是DSP的其他中断如ADC和PWM等可以正常工作。接着我通过开发板的复位按钮复位DSP,然后就能顺利进入SCI接收中断接收到SCI数据。现在我想解决的是一上电,DSP就能接收到SCI数据,而不是通过复位才能接收到上位机下发的数据。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用XDS110仿真器烧录到Flash,并在线仿真运行,上位机发送数据,SCI能进入中断,并接收到完整的数据。当我拔掉仿真器,通过USB重新上电,重新打开串口,并通过上位机发送数据,DSP无法进入SCI接收中断接收到SCI数据,但是DSP的其他中断如ADC和PWM等可以正常工作。接着我通过开发板的复位按钮复位DSP,然后就能顺利进入SCI接收中断接收到SCI数据。现在我想解决的是一上电,DSP就能接收到SCI数据,而不是通过复位才能接收到上位机下发的数据。谢谢!
是的,使用的是TI的开发板库函数例程,通过这两天的调试发现,当使用开发板自带的虚拟端口virtual COM进行SCI通信时。离线跑程序需要按下复位按钮复位DSP,然后才能顺利进入SCI接收中断。如果改用配置GPIO28和GPIO29进行收发,利用外部USB-TLL的串口驱动进行通信时,就没有这个问题,可以直接进行收发。请问这是跟DSP上电时序有关系吗?
如果改用配置GPIO28和GPIO29进行收发,利用外部USB-TLL的串口驱动进行通信时,就没有这个问题,可以直接进行收发。请问这是跟DSP上电时序有关系吗?
是的,我的猜想和您相同。请您具体看一下
5.9.2 Reset Timing