This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: ccs10,用仿真器XDS200连接28377,连不上

Part Number: TMS320F28377D

点击ccxml文件的test connection,出现以下报错信息:

[Start: Texas Instruments XDS2xx USB Onboard Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]
-----[Print the board config pathname(s)]------------------------------------

C:\Users\hasee\AppData\Local\TEXASI~1\CCS\
ti\3\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_io
Failed to open i/o connection (xds2xxu:0)

An error occurred while soft opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.

The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.

[End: Texas Instruments XDS2xx USB Onboard Debug Probe_0]

直接Launch后connect,出现以下错误:

Error initializing emulator:
(Error -2083 @ 0x0)
Unable to communicate with the debug probe. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation.
(Emulation package 9.2.0.00002)

确定仿真器和板子没问题,因为换一台电脑能连上。网上有说是驱动没装好的,但是具体怎么检查不清楚。