Part Number: TMS320F28377D
Other Parts Discussed in Thread: UNIFLASH
CCS10 CCXML配置:TI XDS2XX USB Onboard debug probe
test connection正常,选中CPU1-connect target时报错:
C28xx_CPU1: Trouble Reading Register ST1: (Error -1041 @ 0x5F453) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.2.0.00002)
C28xx_CPU1: GEL: Error while executing OnTargetConnect(): Target failed to read register ST1
at (ST1&~(0x0100)) [f28377d_cpu1.gel:312]
at C28x_Mode() [f28377d_cpu1.gel:88]
at OnTargetConnect()
C28xx_CPU1: Error initializing flash programming: Interface returned from dll, but flash is not available on this device.
C28xx_CPU1: Error: (Error -1135 @ 0x82BF0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.2.0.00002)
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
此时在debug界面,点击“system reset”

会报如下错误:C28xx_CPU1: Failed System Reset: (Error -6306) Failed to connect to PRSC module. (Emulation package 9.2.0.00002)
点击“Reset Emulator”

会报错:C28xx_CPU1: Failed to reset the emulator: An attempt to access the USCIF interface via USCIF ECOM has failed. (Emulation package 9.2.0.00002)