This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I download C2000ware SDK , and we use TMS320F280025C board and the example of TMS320F280025C from SDK .
but when I download code to chip Flash after build project with Flash_lnk.cmd, it reminds dowloaded successful , but the LEDs didn't show any light .
and when I donwload code to chip ram after build project again with Ram_lnk.cmd, and the LEDs lights shine .
I didn't modify anything about the code , just build with Flash_lnk.cmd or Ram_lnk.cmd , but it seems the code didn't load in Flash .
need friends helpful and warmful answers and advice .
Thank you
你好,具体使用的是哪个例程?你是如何操作进行“build with Flash_lnk.cmd or Ram_lnk.cmd”的?
如果是这个位置的LED例程(C:\ti\c2000\C2000Ware_3_04_00_00\driverlib\f28002x\examples\led),有没有尝试过直接选择flash编译?(“编译”按钮小锤子旁边有个倒三角,点击倒三角调出下拉菜单可以看到“flash”编译或者“ram”编译,选择“flash”编译后程序就会进行flash烧写了)
另外可以看一下这个帖子:https://e2echina.ti.com/support/microcontrollers/c2000/f/c2000-microcontrollers-forum/201373/--ram-flash
是的,flash.cmd是通用的,CPU1_LAUNCHXL_FLASH.cmd主要是为了适用于launchPAD的,但其他工程如果内存分配没有重复的话也是适用的。
SDK默认100mHz,可以在device.h中
#define DEVICE_SYSCLK_FREQ ((DEVICE_OSCSRC_FREQ * 30) / (2 * 3 * 1))
部分修改