Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
您好!
我配置了ADCA的SOC0和ADCB的SOC0来进行同步采样,用DMA进行数据的搬移,目前遇到一个问题:只有一个数据被搬移了,而我需要采样32个数据
配置的代码如下:
#pragma DATA_SECTION(AdcaDataU, "ramgs0");
#pragma DATA_SECTION(AdcbDataI, "ramgs0");
Uint16 AdcaDataU[RESULTS_BUFFER_SIZE] = {100}; // 电压采样值
Uint16 AdcbDataI[RESULTS_BUFFER_SIZE] = {100}; // 电流采样值
// ADCINA0、1-->电压U
// ADCINB2、3-->电流I
void Adc_Init()
{
EALLOW;
// Write prescale configurations
// ADC max clock == 50MHz
AdcaRegs.ADCCTL2.bit.PRESCALE = 6; // Set ADCCLK divider to /4
AdcbRegs.ADCCTL2.bit.PRESCALE = 6; // set ADCCLK divider to /4
// Set mode(16位差分输入)
AdcSetMode(ADC_ADCA, ADC_RESOLUTION_16BIT, ADC_SIGNALMODE_DIFFERENTIAL);
AdcSetMode(ADC_ADCB, ADC_RESOLUTION_16BIT, ADC_SIGNALMODE_DIFFERENTIAL);
// SOC0 will convert ADCINA0/A1(ADC_CHANNEL_0/ADC_CHANNEL_1)
AdcaRegs.ADCSOC0CTL.bit.CHSEL = ADC_CHANNEL_0;
AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = 5; // 配置EPWM1A触发
AdcaRegs.ADCSOC0CTL.bit.ACQPS = 39; // 采样时间40 ADC Clock Cycles, (39 ACQPS plus 1)
AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1; // Set pulse positions to late
////////////////////ADC中断设置////////////////////
AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 0; //end of SOC0 will set INT1 flag
AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared
// SOC0 will convert ADCINB2/B3(ADC_CHANNEL_2/ADC_CHANNEL_3)
AdcbRegs.ADCSOC0CTL.bit.CHSEL = ADC_CHANNEL_2;
AdcbRegs.ADCSOC0CTL.bit.TRIGSEL = 5; // 配置EPWM1A触发
AdcbRegs.ADCSOC0CTL.bit.ACQPS = 39; // 采样时间40 ADC Clock Cycles, (39 ACQPS plus 1)
AdcbRegs.ADCCTL1.bit.INTPULSEPOS = 1;
AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1; // Power up the ADC
AdcbRegs.ADCCTL1.bit.ADCPWDNZ = 1;
EDIS;
// Delay for 1ms to allow ADCs time to power up
DELAY_US(1000);
///////////////////////// DMA配置 ///////////////////////
// DMAInitialize - This function initializes the DMA to a known state.
DMAInitialize();
// DMA1
// 配置目标地址和源地址
DMACH1AddrConfig(AdcaDataU, &AdcaResultRegs.ADCRESULT0);
// 每次burst配置成传输1个16bit word,每个word传输完成后,源地址和目标地址都递增0
DMACH1BurstConfig(0, 0, 0);
//每次Teransfer传输RESULTS_BUFFER_SIZE-1个burst,每次burst传输完成后源地址和目标地址递增1
DMACH1TransferConfig((RESULTS_BUFFER_SIZE - 1),1, 1);
DMACH1ModeConfig(
DMA_ADCAINT1, // Source select
PERINT_ENABLE, // Peripheral interrupt enable
ONESHOT_DISABLE, // Oneshot diaable
CONT_ENABLE, // Continuous enable
SYNC_DISABLE,
SYNC_SRC,
OVRFLOW_DISABLE, // Disable the overflow interrupt
SIXTEEN_BIT, // 16-bit data size transfers
CHINT_END, // Generate interrupt to CPU at end of transfer
CHINT_DISABLE // Channel Interrupt to CPU disable
);
// DMA2
DMACH2AddrConfig(AdcbDataI, &AdcbResultRegs.ADCRESULT0);
DMACH2BurstConfig(0, 0, 0);
DMACH2TransferConfig((RESULTS_BUFFER_SIZE - 1), 1, 1);
DMACH2ModeConfig(
DMA_ADCAINT1,
PERINT_ENABLE,
ONESHOT_DISABLE,
CONT_ENABLE,
SYNC_DISABLE,
SYNC_SRC,
OVRFLOW_DISABLE,
SIXTEEN_BIT,
CHINT_END,
CHINT_ENABLE
);
// ADC采样触发(EPWM1SOCA)
EALLOW;
EPwm1Regs.ETSEL.bit.SOCASEL = ET_CTR_ZERO;
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm1Regs.ETPS.bit.SOCAPRD = ET_1ST; // Generate pulse on 1st event
EDIS;
// Start DMA
StartDMACH1();
StartDMACH2();
}
void dmach2_isr(void)
{
while(1)
{
__asm(" NOP");
}
//PieCtrlRegs.PIEACK.all = PIEACK_GROUP7;
}
通过调试发现只有第一次的采样结果正确的保存了,如下所示:

我猜是第一次采样后ADC产生中断标志位后,再触发了DMA的数据转移,一个burst后,由于中断的标志位没有给清除,就没进行下次的数据转移了??
我现在的问题就是:怎么样能够再每次的ADC中断后触发后产生DMA的数据搬移呢?
感谢您的回答!