This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: PWM移相值等于CMPA时,导致AQ设定的CMPA EVENT丢失问题

Part Number: TMS320F280049C


PWM1 UP_DOWN模式,固定50%占空比输出,CMPA_U时SET ,CMPA_D时CLR,在CTR=0时发出同步信号;

PWM2 UP_DOWN模式,固定50%占空比输出,CMPA_U时SET ,CMPA_D时CLR;

PWM2相对于PWM1进行移相,移相值在0~PRD范围.

简单示意图:

测试过程中遇到的问题是,当移相值接近CMPA值时(如,CMPA=100,PHS = 99/100/101),会出现PWM2发出的波形不正常,初步估计是CTR =0时载入PHS值,导致EPWM2在CMPA的动作错过了。

实际测试波形:

请帮我分析一下具体是什么原因,需要怎样解决,谢谢。