This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: PGA采样应用

Part Number: TMS320F280049C

pga_ex1_dac_adc_ext_loopback.c历程中PGA配置

void initPGA(void)
{
//
// Set a gain of 3 to PGA2
//
PGA_setGain(PGA2_BASE, PGA_GAIN_3);

//
// No filter resistor for output
//
PGA_setFilterResistor(PGA2_BASE, PGA_LOW_PASS_FILTER_DISABLED);

//
// Enable PGA2
//
PGA_enable(PGA2_BASE);
}

实际应用PGA有PGA_OF,和PGA_IN两种情况。历程中没有体现这种区别,怎么配置PGA是OUT还是IN

  • 不知我是否对您的疑惑理解正确

    在例程中,有如下说明,硬件上是连接  DACA_OUT (Analog Pin A0) 和  PGA1_IN 

    The output of the DAC is externally connected to PGA1 for a 3x gain amplification. It uses two ADC channels to sample the DAC output and the amplified voltage output from PGA1. The ADC is connected to these signals internally.

    //! - Connect DACA_OUT (Analog Pin A0) to PGA1_IN (Pin 15 on HSEC connector of
    //! - CCard)
    //! - Connect PGA1NEG to GND 

    //! This example generates 400 mV using the DAC output (it uses an internal
    //! voltage reference). The output of the DAC is externally connected to PGA1
    //! for a 3x gain amplification. It uses two ADC channels to sample the
    //! DAC output and the amplified voltage output from PGA1. The ADC is connected
    //! to these signals internally.
    //!
    //! \b External \b Connections \n
    //!  - Connect DACA_OUT (Analog Pin A0) to PGA1_IN (Pin 15 on HSEC connector of 
    //!  - CCard)
    //!  - Connect PGA1NEG to GND