This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: 是否需要使能测试

Part Number: TMS320F280049C


我使用can_ex4_simple_transmit进行测试can发送功能时,

Control_Init(); //控制参数初始化

EINT; //Enable interrupts globally
ERTM;
CAN_enableTestMode(CANA_BASE, CAN_TEST_EXL);  //是否需要使能,can测试模式是环回模式的我觉得应该不用?

//20210730从28037xd移植过来的

CAN_setupMessageObject(CANA_BASE, TX_MSG_OBJ_ID, 0x95555555,
CAN_MSG_FRAME_EXT, CAN_MSG_OBJ_TYPE_TX, 0,
CAN_MSG_OBJ_NO_FLAGS, MSG_DATA_LENGTH);

//
// Initialize the transmit message object data buffer to be sent
//
txMsgData[0] = 0x01;
txMsgData[1] = 0x23;
txMsgData[2] = 0x45;
txMsgData[3] = 0x67;
txMsgData[4] = 0x89;
txMsgData[5] = 0xAB;
txMsgData[6] = 0xCD;
txMsgData[7] = 0xEF;

//