This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: 如何用280049内部flash存储ADC校准数据,就行ST的芯片都可以用内部flash存相关数据。

Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE

如题

  • 你好,C2000系列可以用FlashAPI函数库对芯片内部flash进行实时擦写,具体的你可以看一下该函数的介绍和例程:

    C:\ti\c2000\C2000Ware_3_04_00_00\libraries\flash_api\f28004x

    C:\ti\c2000\C2000Ware_3_04_00_00\driverlib\f28004x\examples\flash

  • 我记得用flashAPI函数,需要把程序搬到ram中运行,不然程序运行时不可以操作flash。我只希望存储ADC校准和设置参数不超过30byte。确定程序运行时调用FLASHapi函数可以把参数写到flash中吗?

  • 能不能回答一下,到底能不能实现啊,要不要把FLASHapi函数搬到ram中运行。我只是希望把30个byte的参数在程序运行时写到内部flash中,不是要bootloader的功能。希望具体回答我饿问题,不要复制链接给我。谢谢。

  • 出于工作需要回复一下,具体问题回复留意新帖。