Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
想以写寄存器的方式进行配置,没有找到
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
想以写寄存器的方式进行配置,没有找到
想以写寄存器的方式进行配置
目前给出的都是driverlib下的例程
写寄存器的话,您可以根据用户指南的寄存器结合driverlib下的例程的I2C配置注释说明来写
您可以参考一下
C:\ti\c2000\C2000Ware_3_04_00_00\driverlib\f2838x\driverlib_cm\inc
下的 hw_i2c.h 以及 C:\ti\c2000\C2000Ware_3_04_00_00\driverlib\f2838x\driverlib_cm 下的i2c文件
这个我看了,这都是封装好的写地址的方式,封装后写的不清不楚的,而且例程太简单了,管脚都没定义,我自己写我想写寄存器的方式,这样方便写,起码CPU以前都是写寄存器的知道怎么写,那个例程看了跟没看似的,没有用
//
// Included Files
//
#include <stdint.h>
#include <stdbool.h>
#include "cm.h"
//
// Defines
//
#define SLAVE_ADDRESS 0x3C
#define NUM_I2C_DATA 3
#define PASS 0
#define FAIL 1
int Ucount;
// Globals
//
uint32_t result = FAIL;
uint32_t ui32DataTx;
static uint32_t ui32DataRx;
//
// Function Prototypes
//
void initI2C(void);
__interrupt void I2C0SlaveIntHandler(void);
//
// Main
//
void main(void)
{
uint16_t i;
//
// disable WD, enable peripheral clocks.
//
CM_init();
//
// Enable the I2C0 interrupt on the processor (NVIC).
//
I2C_registerInt(INT_I2C0,I2C0SlaveIntHandler);
//
// Set I2C use, initializing master and slave
//
initI2C();
//
// Initialize the data to send.
//
ui32DataTx = 'I';
//
// Place the data to be sent in the data register.
//
I2C_putMasterData(I2C0_BASE, ui32DataTx);
//
// Initiate send of single piece of data from the master. Since the
// loopback mode is enabled, the Master and Slave units are connected
// allowing us to receive the same data that we sent out.
//
I2C_setMasterConfig(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);
while(1)
{
//
// Delay
//
for(i=1000; i>0; i--);
Ucount++;if(Ucount>256) Ucount=0;
I2C_putMasterData(I2C0_BASE, Ucount);
I2C_setMasterConfig(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);
}
}
//
// Function to configure I2C0.
//
void initI2C()
{
//
// Enable the Master module.
//
I2C_enableMaster(I2C0_BASE);
//
// I2C configuration. Set up to transfer data at 100 Kbps.
//
I2C_initMaster(I2C0_BASE,I2C_CLK_FREQ,false);
//
// Enable the Slave module.
//
I2C_enableSlave(I2C0_BASE);
//
// Configure for internal loopback mode
//
I2C_setSlaveAddress(I2C0_BASE,SLAVE_ADDRESS,I2C_MASTER_WRITE);
I2C_setOwnSlaveAddress(I2C0_BASE,I2C_SLAVE_ADDR_PRIMARY,SLAVE_ADDRESS);
// I2C_enableLoopback(I2C0_BASE);
//
// Configure and turn on the I2C0 slave interrupt. The I2C_enableSlaveInt()
// gives you the ability to only enable specific interrupts. For this case
// we are only interrupting when the slave device receives data.
//
I2C_enableSlaveInt(I2C0_BASE);
}
//
// I2C0 Receive ISR.
//
__interrupt void I2C0SlaveIntHandler(void)
{
uint32_t slvStatus;
//
// Get the slave interrupt status
//
slvStatus = I2C_getSlaveIntStatus(I2C0_BASE,I2C_MASTER_RAW_INT);
//
// Clear the I2C0 interrupt flag.
//
I2C_clearSlaveInt(I2C0_BASE);
//
// Read the data from the slave.
//
ui32DataRx = I2C_getSlaveData(I2C0_BASE);
if(ui32DataRx != ui32DataTx)
result = FAIL;
else
result = PASS;
//
// Clear the slave interrupt status
//
I2C_clearSlaveIntSource(I2C0_BASE,slvStatus);
}
//
// End of File
//
//#############################################################################
//
// FILE: cm_common_config_c28x.c
//
// TITLE: C28x Common Configurations to be used for the CM Side.
//
//! \addtogroup driver_example_list
//! <h1>C28x Common Configurations</h1>
//!
//! This example configures the GPIOs and Allocates the shared peripherals
//! according to the defines selected by the users.
//!
//
//#############################################################################
// $TI Release: F2838x Support Library v3.04.00.00 $
// $Release Date: Fri Feb 12 19:08:49 IST 2021 $
// $Copyright:
// Copyright (C) 2021 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
void main(void)
{
//
// Initialize device clock and peripherals
//
Device_init();
//
// Boot CM core
//
#ifdef _FLASH
Device_bootCM(BOOTMODE_BOOT_TO_FLASH_SECTOR0);
#else
Device_bootCM(BOOTMODE_BOOT_TO_S0RAM);
#endif
//
// Disable pin locks and enable internal pull-ups.
//
Device_initGPIO();
GPIO_setPinConfig(GPIO_31_CM_I2CA_SDA);
GPIO_setPinConfig(GPIO_32_CM_I2CA_SCL);
GPIO_setPadConfig(45, GPIO_PIN_TYPE_STD);
GPIO_setPinConfig(GPIO_45_GPIO45);
GPIO_setDirectionMode(45, GPIO_DIR_MODE_OUT);
GPIO_setMasterCore(45, GPIO_CORE_CM);
#ifdef ETHERNET
//
// Set up EnetCLK to use SYSPLL as the clock source and set the
// clock divider to 2.
//
// This way we ensure that the PTP clock is 100 MHz. Note that this value
// is not automatically/dynamically known to the CM core and hence it needs
// to be made available to the CM side code beforehand.
SysCtl_setEnetClk(SYSCTL_ENETCLKOUT_DIV_2, SYSCTL_SOURCE_SYSPLL);
//
// Configure the GPIOs for ETHERNET.
//
//
// MDIO Signals
//
GPIO_setPinConfig(GPIO_105_ENET_MDIO_CLK);
GPIO_setPinConfig(GPIO_106_ENET_MDIO_DATA);
//
// Use this only for RMII Mode
//GPIO_setPinConfig(GPIO_73_ENET_RMII_CLK);
//
//
//MII Signals
//
GPIO_setPinConfig(GPIO_109_ENET_MII_CRS);
GPIO_setPinConfig(GPIO_110_ENET_MII_COL);
GPIO_setPinConfig(GPIO_75_ENET_MII_TX_DATA0);
GPIO_setPinConfig(GPIO_122_ENET_MII_TX_DATA1);
GPIO_setPinConfig(GPIO_123_ENET_MII_TX_DATA2);
GPIO_setPinConfig(GPIO_124_ENET_MII_TX_DATA3);
//
//Use this only if the TX Error pin has to be connected
//GPIO_setPinConfig(GPIO_46_ENET_MII_TX_ERR);
//
GPIO_setPinConfig(GPIO_118_ENET_MII_TX_EN);
GPIO_setPinConfig(GPIO_114_ENET_MII_RX_DATA0);
GPIO_setPinConfig(GPIO_115_ENET_MII_RX_DATA1);
GPIO_setPinConfig(GPIO_116_ENET_MII_RX_DATA2);
GPIO_setPinConfig(GPIO_117_ENET_MII_RX_DATA3);
GPIO_setPinConfig(GPIO_113_ENET_MII_RX_ERR);
GPIO_setPinConfig(GPIO_112_ENET_MII_RX_DV);
GPIO_setPinConfig(GPIO_44_ENET_MII_TX_CLK);
GPIO_setPinConfig(GPIO_111_ENET_MII_RX_CLK);
//
//Power down pin to bring the external PHY out of Power down
//
GPIO_setDirectionMode(108, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(108, GPIO_PIN_TYPE_PULLUP);
GPIO_writePin(108,1);
//
//PHY Reset Pin to be driven High to bring external PHY out of Reset
//
GPIO_setDirectionMode(119, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(119, GPIO_PIN_TYPE_PULLUP);
GPIO_writePin(119,1);
#endif
#ifdef MCAN
//
// Setting the MCAN Clock.
//
SysCtl_setMCANClk(SYSCTL_MCANCLK_DIV_4);
//
// Configuring the GPIOs for MCAN.
//
GPIO_setPinConfig(DEVICE_GPIO_CFG_MCANRXA);
GPIO_setPinConfig(DEVICE_GPIO_CFG_MCANTXA);
#endif
#ifdef CANA
//
// Configuring the GPIOs for CAN A.
//
GPIO_setPinConfig(DEVICE_GPIO_CFG_CANRXA);
GPIO_setPinConfig(DEVICE_GPIO_CFG_CANTXA);
//
// Allocate Shared Peripheral CAN A to the CM Side.
//
SysCtl_allocateSharedPeripheral(SYSCTL_PALLOCATE_CAN_A,0x1U);
#endif
#ifdef CANB
//
// Configuring the GPIOs for CAN B.
//
GPIO_setPinConfig(DEVICE_GPIO_CFG_CANRXB);
GPIO_setPinConfig(DEVICE_GPIO_CFG_CANTXB);
//
// Allocate Shared Peripheral CAN B to the CM Side.
//
SysCtl_allocateSharedPeripheral(SYSCTL_PALLOCATE_CAN_B,0x1U);
#endif
#ifdef UART
//
// Configure GPIO85 as the UART Rx pin.
//
GPIO_setPinConfig(GPIO_85_UARTA_RX);
GPIO_setDirectionMode(85, GPIO_DIR_MODE_IN);
GPIO_setPadConfig(85, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(85, GPIO_QUAL_ASYNC);
//
// Configure GPIO84 as the UART Tx pin.
//
GPIO_setPinConfig(GPIO_84_UARTA_TX);
GPIO_setDirectionMode(84, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(84, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(84, GPIO_QUAL_ASYNC);
#endif
#ifdef USB
#ifdef USE_20MHZ_XTAL
//
// Set up the auxiliary PLL so a 60 MHz output clock is provided to the USB module.
// This fixed frequency is required for all USB operations.
//
SysCtl_setAuxClock(SYSCTL_AUXPLL_OSCSRC_XTAL |
SYSCTL_AUXPLL_IMULT(48) |
SYSCTL_REFDIV(2U) | SYSCTL_ODIV(4U) |
SYSCTL_AUXPLL_DIV_2 |
SYSCTL_AUXPLL_ENABLE |
SYSCTL_DCC_BASE_0);
#else
//
// Set up the auxiliary PLL so a 60 MHz output clock is provided to the USB module.
// This fixed frequency is required for all USB operations.
//
SysCtl_setAuxClock(SYSCTL_AUXPLL_OSCSRC_XTAL |
SYSCTL_AUXPLL_IMULT(48) |
SYSCTL_REFDIV(2U) | SYSCTL_ODIV(5U) |
SYSCTL_AUXPLL_DIV_2 |
SYSCTL_AUXPLL_ENABLE |
SYSCTL_DCC_BASE_0);
#endif
//
// Allocate Shared Peripheral USB to the CM Side.
//
SysCtl_allocateSharedPeripheral(SYSCTL_PALLOCATE_USBA, 1);
GPIO_setPinConfig(GPIO_0_GPIO0);
GPIO_setPadConfig(0, GPIO_PIN_TYPE_STD);
GPIO_setDirectionMode(0, GPIO_DIR_MODE_OUT);
GPIO_setMasterCore(0, GPIO_CORE_CM);
//
// Set the master core of GPIOs to CM.
//
GPIO_setMasterCore(42, GPIO_CORE_CM);
GPIO_setMasterCore(43, GPIO_CORE_CM);
GPIO_setMasterCore(46, GPIO_CORE_CM);
GPIO_setMasterCore(47, GPIO_CORE_CM);
GPIO_setMasterCore(120, GPIO_CORE_CM);
GPIO_setMasterCore(121, GPIO_CORE_CM);
//
// Set the USB DM and DP GPIOs.
//
GPIO_setAnalogMode(42, GPIO_ANALOG_ENABLED);
GPIO_setAnalogMode(43, GPIO_ANALOG_ENABLED);
//
// Set the direction for VBUS and ID.
//
GPIO_setDirectionMode(46, GPIO_DIR_MODE_IN);
GPIO_setDirectionMode(47, GPIO_DIR_MODE_IN);
//
// Configure the Power Fault.
//
GPIO_setMasterCore(120, GPIO_CORE_CM);
GPIO_setDirectionMode(120, GPIO_DIR_MODE_IN);
//
// Configure the External Power Signal Enable.
//
GPIO_setMasterCore(121, GPIO_CORE_CM);
GPIO_setDirectionMode(121, GPIO_DIR_MODE_OUT);
GPIO_writePin(121, 1);
//
// Set the CM Clock to run at 120MHz.
// The CM Clock is a fractional multiple of the AUXPLL Clock (120 Mhz) from
// which the USB Clock (60 MHz) is derived.
//
SysCtl_setCMClk(SYSCTL_CMCLKOUT_DIV_1, SYSCTL_SOURCE_AUXPLL);
#endif
}
就是这个例程简单的改了一下连续发送,
问题1:禁止I2C_enableLoopback(I2C0_BASE);为什么还能进接收中断
问题2:为什么测试32管教没有波形
问题3:想确定这里的解释有没有写反,为什么I2C_MASTER_WRITE是读 那个是写