This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: epwmXbar的应用问题,根据手册配置寄存器后没办法触发事件

Part Number: TMS320F28388D

如题,想通过输入类型的GPIO88,然后经过InputXbar然后到EpwmXbar然后通过Trip4到ePwmModules,发现怎么都触发不了:

CPU1配置Xbar:

EALLOW;

InputXbarRegs.INPUT12SELECT = 88;

EPwmXbarRegs.TRIP4MUXENABLE.BIT.MUX27 = 1;

EPwmXbarRegs.TRIP4MUX16TO31CFG.BIT.MUX27 = 1;

EPwmXbarRegs.TRIPOUTINV.BIT.TRIP4 = 1;

EDIS;

cpu2配置触发信号:

EALLOW;

EPwm1Regs.TZSEL.BIT.DCAEVTA =1;

EPwm1Regs.DCTRIPSEL.BIT.DCALCOMPSEL = 4;

EPwm1Regs.TZDCSEL.BIT.DCAEVT1 = 3;//GPIO低电平触发

EPwm1Regs.DCACTL.BIT.EVT1SRCSEL = 0;

EPwm1Regs.DCACTL.BIT.EVT1FRCSYNCSEL = 1;

EPwm1Regs.DCACTL.BIT.EVT1LATSEL = 0;

EPwm1Regs.TZCTL.BIT.DCAEVT1 = 1;

EPwm1Regs.TZCTL2.BIT.ETZE= 0;

EPwm1Regs.TZCTL.BIT.TZA = 1;

EPwm1Regs.TZCTL.BIT.TZB = 1;

EDIS;

gpio88已经配置好上拉,在仿真上可以看到信号正常翻转了,但是在EPwm1Regs.TZOSTFLG.BIT.DCAEVT1一直是0,也就是说没有触发到事件。我想问一下我上面的配置有问题吗?我用TZ3直接触发OST1是没有问题的,现在用上epwmXbar做转接不知道那出错了,也没能找到相关例程,希望大神门指教一下