上图为bissc例程文档,物理上SPI单元FIFO的宽度是16位宽的
但是这里的SPI_FIFO_WIDTH宏定义设置为了12,这是为什么呢
这个宏参数是不是要配置给CLB单元呢?
注释中“Optimal character length”是指这个12bit的fifo宽度便于CLB单元做处理吗?
如果是位置数据26位 1个起始位 1和CDS位 1个错误位 1个警告位 6个CRC位,那么一帧数据是36bit,这和SPI_FIO_WIDTH设置为12有什么关系呢 怎么就说是优化的字符宽度呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

上图为bissc例程文档,物理上SPI单元FIFO的宽度是16位宽的
但是这里的SPI_FIFO_WIDTH宏定义设置为了12,这是为什么呢
这个宏参数是不是要配置给CLB单元呢?
注释中“Optimal character length”是指这个12bit的fifo宽度便于CLB单元做处理吗?
如果是位置数据26位 1个起始位 1和CDS位 1个错误位 1个警告位 6个CRC位,那么一帧数据是36bit,这和SPI_FIO_WIDTH设置为12有什么关系呢 怎么就说是优化的字符宽度呢
我的理解是“Optimal character length”应该是指根据编码器和需要发送的bit数量设置的最佳字符长度,但是具体这个数值怎么设置,我查了文档和论坛都没有找到相关资料。可能得咨询E2E的工程师才能得到比较完整的说明。
好的 感谢帮助
再请问bissc库 用到了GPIO6和GPIO7 这两个引脚涉及到ePWM4 例程中使能了ePWM4的时钟
可是我没有发现ePWM3涉及到例程中的什么应用 bissc库用到ePWM3了吗
应该来说biss-c库只需要一个eWM模块就够了,例程和说明文档中也只是使能了ePWM3的时钟,但是没看到哪里有使用ePWM3的。