你好,问:280049 外设LIN用作SCI,系统主频100M, 要9600波特率,相关对应BRSR.SCI_LIN_PSL,SCI_LIN_PSH, M值应该多少?怎样计算?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,问:280049 外设LIN用作SCI,系统主频100M, 要9600波特率,相关对应BRSR.SCI_LIN_PSL,SCI_LIN_PSH, M值应该多少?怎样计算?
您可以看一下driverlib内的如下函数
//***************************************************************************** // //! Set Baud Rate Prescaler //! //! \param base is the LIN module base address //! \param prescaler is the 24-bit integer prescaler //! \param divider is the 4-bit fractional divider //! //! In LIN and SCI mode, this function is used to set the baudrate based on //! the \e prescaler and \e divider values. //! //! P = Prescaler \n //! M = Fractional Divider \n //! Bitrate = (SYSCLOCK) / ((P + 1 + M/16) * 16) \n //! //! \return None. // //***************************************************************************** static inline void LIN_setBaudRatePrescaler(uint32_t base, uint32_t prescaler, uint32_t divider) { // // Check the arguments. // ASSERT(LIN_isBaseValid(base)); ASSERT(prescaler <= (LIN_BRSR_SCI_LIN_PSL_M | LIN_BRSR_SCI_LIN_PSH_M)); ASSERT(divider <= (LIN_BRSR_M_M >> LIN_BRSR_M_S)); // // Set baud rate prescaler and divider // HWREG_BP(base + LIN_O_BRSR) = (prescaler | (divider << LIN_BRSR_M_S)); }
波特率配置没问题了。谢谢
1、参考例程(地址方式)配置或修改LIN收发都可以正常
2、参考例程(地址方式)配置LIN,自己写配置LIN模块相关(时钟+PIN+LIN的SCI模式配置)代码,配置成内循环或外循环,接收用查询或中断都收和发不成功,是什么原因?出错在哪里?
配置LIN代码如下:
EALLOW;
LinaRegs.SCIGCR0.bit.RESET = 0; // Into reset, lin module
DELAY_US(50);
LinaRegs.SCIGCR0.bit.RESET = 1; // Out of reset
LinaRegs.SCIGCR1.bit.SWnRST = 0; // Into software reset, reset state
//
// SCI Configurations
//
LinaRegs.SCIGCR1.bit.COMMMODE = 0; // Idle-Line Mode 1
LinaRegs.SCIGCR1.bit.TIMINGMODE = 1; // Asynchronous Timing 1
LinaRegs.SCIGCR1.bit.PARITYENA = 0; // No Parity Check 1
LinaRegs.SCIGCR1.bit.PARITY = 0; // Odd Parity 1
LinaRegs.SCIGCR1.bit.STOP = 0; // One Stop Bit 1
LinaRegs.SCIGCR1.bit.CLK_MASTER = 1; // Enable SCI Clock 1
LinaRegs.SCIGCR1.bit.LINMODE = 0; // SCI Mode
LinaRegs.SCIGCR1.bit.SLEEP = 0; // Ensure Out of Sleep
LinaRegs.SCIGCR1.bit.MBUFMODE = 0; // No Buffers Mode 1
LinaRegs.SCIGCR1.bit.LOOPBACK = 0; // External Loopback
// LinaRegs.SCIGCR1.bit.LOOPBACK = 1; // interner Loopback
LinaRegs.SCIGCR1.bit.CONT = 1; // Continue on Suspend 1
// LinaRegs.SCIGCR1.bit.RXENA = 1; // Enable RX
// LinaRegs.SCIGCR1.bit.TXENA = 1; // Enable TX
//
// Ensure IODFT is disabled
//
// LinaRegs.IODFTCTRL.bit.IODFTENA = 0x0;
//
// Set transmission length
//
LinaRegs.SCIFORMAT.bit.CHAR = 7; //Eight bits 1
LinaRegs.SCIFORMAT.bit.LENGTH = 0; //One byte 1
//
// Set baudrate
//
LinaRegs.BRSR.bit.SCI_LIN_PSL = 650; //Baud = 9600 bps
LinaRegs.BRSR.bit.M = 1;
LinaRegs.SCIGCR1.bit.SWnRST = 1; //bring out of software reset, ready state
//-----------int---------------------------------
LinaRegs.SCISETINT.bit.SETRXINT = 1;
LinaRegs.SCICLEARINTLVL.bit.CLRRXINTLVL = 1;
// LinaRegs.SCISETINTLVL.bit.SETRXINTOVO = 1;
LinaRegs.LIN_GLB_INT_EN.bit.GLBINT0_EN = 1; //enable
LinaRegs.LIN_GLB_INT_CLR.bit.INT0_FLG_CLR = 1; //clear int0
LinaRegs.LIN_GLB_INT_FLG.bit.INT0_FLG = 1; //clear flag
//
// Disable write to protected registers
//
EDIS;
自己写配置LIN模块相关(时钟+PIN+LIN的SCI模式配置)代码,配置成内循环或外循环,接收用查询或中断都收和发不成功
请问具体表现是什么?另外您硬件方面使用的是开发板?
自写代码为什么收发不了,表现:Tx示波器没有波形和串口上位没有数据,接收没有中断或查询接收标志RXRDY没有置位
同样TI开发板,lib lin例程库上修改成中断或查询,内循环或外部都正常收发波形和数据。
图2 寄存器异常,什么原因
在上面代码基础上插入LIN例程仿真结果值
//----------------------------------------------
LinaRegs.SCIGCR0.all = 0x00000001; // 插入例程仿真结果值
LinaRegs.SCIGCR1.all = 0x00A20000;
LinaRegs.SCIGCR2.all = 0x030200A2;
LinaRegs.SCISETINT.all = 0x00000302;
LinaRegs.SCICLEARINT.all = 0x00000000;
LinaRegs.SCISETINTLVL.all= 0x00000000;
LinaRegs.SCICLEARINTLVL.all= 0x00000000;
LinaRegs.SCIFLR.all = 0x00000000; // 插入例程仿真结果值
//----------------------------------------------
LinaRegs.SCIGCR1.bit.SWnRST = 1; //bring out of software reset, ready state
1、仿真跑到次位置看寄存器值与插入配置对应值不一样,见图2,为什么会这样?CCS V10.3
2、同个东西,在两页显示不一样为什么会这样?见下两图