This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMPPTKIT开发套件 相关问题



我现在尝试使用build 3,遇到了一些问题

1.

根据说明,我忽略这行

 Start_DC_DC=1;//Start DC-DC MPPT provided LLC PWM is ON(This is checked in the 20kHz SECONDARY ISR)

但是我用的是DC supply 不是PV panel emulator,我拥有的load resistor 是900Ohm,那么我需要将input voltage& current设定为多少才会让power < 165W并且让mppt.incc启动 ?

 

2.

请问说明当中提及的CNTL_2P2Z 和ADC有50KHz的频率,这应该是运算的频率吧? 如果我想要修改的话,该由哪边着手?