This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: 程序烧录问题

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE

工程师,您好:

       我将C2000ware中的SDFM程序烧录到28379D时报错:

       C28xx_CPU1: Trouble Reading Register PC: (Error -1156 @ 0x0) Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device. (Emulation package 9.3.0.00042)

        仿真器应该是没问题的,test connection通过;

        jtag 的5引脚是3.3V电平;

        XCLKOUT 引脚是2V,50M的波形;

        请问为什么烧录程序会报错?