Part Number: TMS320F28035
请问一下:28035 芯片 由内部晶振 改为20M外部晶振除了修改这些地方还要修改其他吗


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您可以看一下该函数
//
// XtalOscSel - This function switches to External CRYSTAL oscillator and turns
// off all other clock sources to minimize power consumption. This option may
// not be available on all device packages
//
void
XtalOscSel (void)
{
EALLOW;
SysCtrlRegs.CLKCTL.bit.XTALOSCOFF = 0; // Turn on XTALOSC
DELAY_US(1000L); // 1mS delay to ensure crystal
// oscillator is up and running.
// Adjust as needed.
SysCtrlRegs.CLKCTL.bit.XCLKINOFF = 1; // Turn off XCLKIN
SysCtrlRegs.CLKCTL.bit.OSCCLKSRC2SEL = 0; // Switch to external clock
//
// Switch INTOSC1 to INTOSC2/ext clk
//
SysCtrlRegs.CLKCTL.bit.OSCCLKSRCSEL = 1;
SysCtrlRegs.CLKCTL.bit.WDCLKSRCSEL = 0; // Clock Watchdog off of INTOSC1
SysCtrlRegs.CLKCTL.bit.INTOSC2OFF = 1; // Turn off INTOSC2
SysCtrlRegs.CLKCTL.bit.INTOSC1OFF = 0; // Leave INTOSC1 on
EDIS;
}外部有源晶振
抱歉,刚才没有注意。那您是否有参考例程内的下面函数?您现在是遇到了什么问题?
//
// ExtOscSel - This function switches to External oscillator and turns off all
// other clock sources to minimize power consumption.
//
void
ExtOscSel (void)
{
EALLOW;
//
// 1-GPIO19 = XCLKIN, 0-GPIO38 = XCLKIN
//
SysCtrlRegs.XCLK.bit.XCLKINSEL = 1;
SysCtrlRegs.CLKCTL.bit.XTALOSCOFF = 1; //Turn on XTALOSC
SysCtrlRegs.CLKCTL.bit.XCLKINOFF = 0; //Turn on XCLKIN
SysCtrlRegs.CLKCTL.bit.OSCCLKSRC2SEL = 0; //Switch to external clock
//
// Switch INTOSC1 to INTOSC2/ext clk
//
SysCtrlRegs.CLKCTL.bit.OSCCLKSRCSEL = 1;
SysCtrlRegs.CLKCTL.bit.WDCLKSRCSEL = 0; //Clock Watchdog off of INTOSC1
SysCtrlRegs.CLKCTL.bit.INTOSC2OFF = 1; //Turn off INTOSC2
SysCtrlRegs.CLKCTL.bit.INTOSC1OFF = 0; //Leave INTOSC1 on
EDIS;
}