Part Number: TMS320F28377D
各位专家好,最近我在用TMS320F28377D对EPWM进行配置,一开始出现了EPWM9-12对应引脚没有输出的问题,但是之后查看论坛发现这几位EPWM对应的引脚的配置和之前不一样,然后该问题解决了。
之后,我又遇到了两个很奇怪的问题:
1.EPWM7和EPWM8对应的输出引脚的输出波形很奇怪,有畸变,不是标准方波,具体如下图所示:

2.EPWM11和EPWM12输出电压只有250mv,具体如下图所示:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28377D
各位专家好,最近我在用TMS320F28377D对EPWM进行配置,一开始出现了EPWM9-12对应引脚没有输出的问题,但是之后查看论坛发现这几位EPWM对应的引脚的配置和之前不一样,然后该问题解决了。
之后,我又遇到了两个很奇怪的问题:
1.EPWM7和EPWM8对应的输出引脚的输出波形很奇怪,有畸变,不是标准方波,具体如下图所示:

2.EPWM11和EPWM12输出电压只有250mv,具体如下图所示:

1、你的PWM输出引脚有没有接后端电路?如果有的话可能会受后端电路影响造成畸变。
2、有没有可能是你的示波器探针没有x10?或者示波器设置中没有将数值x10?测量其他波形正常吗?波形是你设置的波形吗?
图1的波形感觉是引脚电容导致的,但是你也提到引脚外部没有接其他外部电路。
图2就完全很莫名了,这个电压值都不能算是高电平(一般0.7V以上认为是能判断为高电平),如果不看幅值的话,波形的频率、占空比是符合输出要求的吗?
建议有条件的话还是用官方的例程来测试一下其他芯片。