This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8412-C2-KIT 无法运行,无法刷入

Other Parts Discussed in Thread: CONTROLSUITE, DRV8412

买了套 DRV8412-C2-KIT,运行DRV8412GUIv9.exe后,步进电机没反应,DC BUS的电压指示也没显示正确的电压,自己重新刷附送的U盘的DRV8412GUIv9.out,刷不进去。

我自己去查了英文的论坛,有人也碰到GUI没反应的问题,最后说是用GUIv5.exe就可以了,可是我的U盘只有v2和v9,v2无法运行,controlSUITE安装后也和U盘一样只有v2和v9,文件夹里的说明是“RevG DRV8412 board should be using v6.out and .exe”,可是哪里有v6啊?

用CCS4、CCS5分别编译GUI_project这个工程也编译不了,搞了两天了,各种版本的软件程序,很晕啊。v5和v6的版本TI官网也找不到了,请问谁能发个v5或v6的GUI和OUT文件给我试试看能否让电机动起来先?谢谢了!

这是用CCS4刷DRV8412GUIv9.out时提示的错误信息:

Device Calibration not complete, check if device is unlocked and recalibrate.
C28xx: Flash Programmer: Device is locked or not connected. Operation cancelled.
C28xx: Trouble Writing Memory Block at 0x3f4925 on Page 0 of Length 0x225
Cannot write to target

  • 应该不是.out文件的问题,不知道你有没有看一下DRV8412-C2-KIT_HowToRunGuide.pdf, 和DRV8412-C2-KIT_HWGuide.pdf, 现将硬件设计好,我觉得很有可能是因为硬件没配置好,导致芯片连接不上。

    Eric

  • 原来GUI和CCS4都能连接上的,但是GUI没有读到板上的数据,CCS刷入时出错,我帖子上有写出错的信息。

    我是看到这个帖子,感觉我的问题和他一样。那些硬件设置也没多复杂,按照说明书一步一步做,检查了很多次的。

    http://e2e.ti.com/support/applications/motor_drivers/f/38/t/142090.aspx

    冲着contolsuit里面还有一个文档写着这个信息,那个v6又没有提供,综合考虑,我只能怀疑是官方给的软件有问题了。

    The GUIv#.out and v#.exe are tied to each other as well as to a DRV8412 board revision.

    RevG DRV8412 board should be using v6.out and .exe

    RevF DRV8412 board should be using v2.out and .exe

    To flash a controlCARD please use CCSv4HowToFlashcontrolCARDS.txt found in this same directory.