Part Number: TMS320F280049C
Other Parts Discussed in Thread: TIDM-1007, SFRA, C2000WARE
您好!
使用F280049 controlCARD 运行ttplpfc的lab1例程,仿真运行正常,重新上电后程序无法运行,S1的开关设置在Flash运行状态(up,up);请问是否需要设置其他参数。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用F280049 controlCARD 运行ttplpfc的lab1例程
请问测试其他例程是否也能复现这样的现象?
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to Flash" bootloader mode */
BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x0000F5, length = 0x00030B
RAMLS2LS3LS4LS5 : origin = 0x009000, length = 0x002000
RAMLS6 : origin = 0x00B000, length = 0x000800
RAMGS0GS1 : origin = 0x00C000, length = 0x002000
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
/* BANK 0 */
FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x000FFE /* on-chip Flash */
FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000 /* on-chip Flash */
/* BANK 1 */
FLASH_BANK1_SEC0 : origin = 0x090000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC1 : origin = 0x091000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC2 : origin = 0x092000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC3 : origin = 0x093000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC4 : origin = 0x094000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC5 : origin = 0x095000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC6 : origin = 0x096000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC7 : origin = 0x097000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC8_9_10 : origin = 0x098000, length = 0x03000 /* on-chip Flash */
FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x001000 /* on-chip Flash */
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x0000F3 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMLS0LS1 : origin = 0x008000, length = 0x001000
RAMLS7 : origin = 0x00B800, length = 0x000800
RAMGS2 : origin = 0x010000, length = 0x002000
RAMGS3 : origin = 0x012000, length = 0x002000
}
SECTIONS
{
codestart : > BEGIN, PAGE = 0, ALIGN(4)
.text : >>FLASH_BANK0_SEC1 | FLASH_BANK0_SEC2 | FLASH_BANK0_SEC3, PAGE = 0, ALIGN(4)
.cinit : > FLASH_BANK1_SEC8_9_10, PAGE = 0, ALIGN(4)
.init_array : > FLASH_BANK0_SEC1, PAGE = 0, ALIGN(4)
.switch : > FLASH_BANK0_SEC1, PAGE = 0, ALIGN(4)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.stack : > RAMM1, PAGE = 1
.data : > RAMLS0LS1, PAGE = 1
.bss : >> RAMGS3 PAGE = 1
.sysmem : > RAMGS2 PAGE = 1
.const : > FLASH_BANK0_SEC4, PAGE = 0, ALIGN(4)
GROUP
{
.TI.ramfunc
{
-l sfra_f32_tmu_eabi.lib
}
ramfuncs
dclfuncs
} LOAD = FLASH_BANK0_SEC6,
RUN = RAMGS0GS1,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
SFRA_F32_Data : > RAMGS2, ALIGN = 64, PAGE = 1
SFRA_Data : > RAMGS2, ALIGN = 64, PAGE=1
FPUmathTables : > FLASH_BANK1_SEC0, PAGE =0
.scratchpad : > RAMLS0LS1, PAGE = 1
.bss_cla : > RAMLS0LS1, PAGE = 1
controlVariables : > RAMLS0LS1, PAGE = 1
.const_cla : LOAD = FLASH_BANK1_SEC8_9_10,
RUN = RAMLS2LS3LS4LS5,
RUN_START(Cla1ConstRunStart),
LOAD_START(Cla1ConstLoadStart),
LOAD_SIZE(Cla1ConstLoadSize),
PAGE = 0
GROUP
{
isrcodefuncs
dclfuncs
} LOAD = FLASH_BANK1_SEC8_9_10,
RUN = RAMLS2LS3LS4LS5,
LOAD_START(isrcodefuncsLoadStart),
LOAD_SIZE(isrcodefuncsLoadSize),
LOAD_END(isrcodefuncsLoadEnd),
RUN_START(isrcodefuncsRunStart),
RUN_SIZE(isrcodefuncsRunSize),
RUN_END(isrcodefuncsRunEnd),
PAGE = 0, ALIGN(4)
/* CLA specific sections */
Cla1Prog : LOAD = FLASH_BANK1_SEC8_9_10,
RUN = RAMLS2LS3LS4LS5,
LOAD_START(Cla1ProgLoadStart),
RUN_START(Cla1ProgRunStart),
LOAD_SIZE(Cla1ProgLoadSize),
PAGE = 0, ALIGN(4)
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
例程中有LED闪烁功能
我指的是 C2000Ware_3_04_00_00\device_support\f2838x\examples\cpu1\led 例程
3_02_00_00版本TIDM-2008/TIDM-1007导入ccs可以运行,C2000Ware_DigitalPower_SDK_3_01_00_00版本程序导入不能运行只能仿真。
新版本的更新情况如下
https://dev.ti.com/tirex/explore/node?node=AIZYaInRZYPdHOEarfi21g__5C6SEVO__LATEST
目前在最新版本内没有TIDM-1007的相关更新
我会在之后拿launchpad来测试一下。