This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您可以看一下
7.8.4.1 Example 1: Initialization Code for Data Logging With Word Counter
Section 7.8.4.1 shows how to log 20 32-bit words, starting at address 00 010016 in data memory.
那我的数据是从哪里来的,或者说最后去了哪里,我该在哪里查看该数据?
Data logging enables the C28x to send selected memory values to a host processor using the standard JTAG port and an XDS510 or other compatible scan controller. You control data logging activity with your application code.
Data logging使 C28x 能够使用标准将选定的内存值发送到主机处理器JTAG 端口和 XDS510 或其他兼容的扫描控制器。
通过查看DMA_CNTRL 来确认是否完成传输完成。您可以使用CCS的memory browser来查看放在00 010016起始地址的数据
目前来看这个功能用的比较少。