Part Number: TMS320F28027
Other Parts Discussed in Thread: C2000WARE
CPUTIMER1ENCLK 复位的时候R/W-1,The CPU Timer 1 is clocked
TIMERxTCR Register 的TSS位 R/W-0 Reads of 0 indicate the CPU-timer is running.To start or restart the CPU-timer, set TSS to 0. At reset, TSS is cleared to 0 and the CPU-timer immediately starts.
按照手册所说定时器1复位后是运行状态的 难道上电的时候要先禁止T1的使能位才能保证时间的正常运行?
还有我目前的程序以T1做100us中断,中断中程序比较多但总体执行时间不会超过中断的时间,这样是否合理?是否影响了中断机制?
此外我想自己定义变量使用,CMD命令给数组和结构体分配空间我看到了,那怎么利用CMD给单一变量或者多个变量指定空间还是编译器自动分配了空间?
谢谢!