Part Number: TMS320F2812
如题,2812在正常工作时,EMU1是3.3的高电平,此时当引脚单独示波器时,DSP挂起,重新上电才能工作;
后来发现,在2812正常工作时,当将EMU1接GND时,就会导致DSP挂起.
想问一下:2812正常工作时,EMU1的逻辑变化会造成2812进入某些状态吗?
另外,EMU1引脚是不是特别敏感?
这些在2812datasheet上没有查到
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F2812
如题,2812在正常工作时,EMU1是3.3的高电平,此时当引脚单独示波器时,DSP挂起,重新上电才能工作;
后来发现,在2812正常工作时,当将EMU1接GND时,就会导致DSP挂起.
想问一下:2812正常工作时,EMU1的逻辑变化会造成2812进入某些状态吗?
另外,EMU1引脚是不是特别敏感?
这些在2812datasheet上没有查到
这个引脚在datasheet上有这样说明:
Emulator pin 1. When TRST is driven high, this pin is used as an interrupt to or from the emulator system and is defined as input/output through the JTAG scan. This pin is also used to put the device into boundary-scan mode. With the EMU0 pin at a logic-high state and the EMU1 pin at a logic-low state, a rising edge on the TRST pin would latch the device into boundary-scan mode. NOTE: An external pullup resistor is recommended on this pin. The value of this resistor should be based on the drive strength of the debugger pods applicable to the design. A 2.2-kΩ to 4.7-kΩ resistor is generally adequate. Since this is application-specific, it is recommended that each target board be validated for proper operation of the debugger and the application.
你的板子上这个引脚有接上拉电阻吗?
哎,找了一圈没找到boundary-scan mode的资料,我也没研究过边界扫描,建议你将问题发送到英文E2E论坛咨询一下,那边会有BU级别的工程师可能会知道这方面的情况:e2e.ti.com/.../c2000-microcontrollers-forum