现有系统的MCBSP接口已经被占用,无法引出
只能通过SPI接口与DA进行通讯
但是SPI接口最大一次只能发送16位数据,而使用FIFO发送的话必须持续写数据否则就会一直进入中断并且CLK信号会持续输出
请问是否有办法实现类似猝发通信那样的功能?TXFIFO的堆栈是必须开启TX的FIFO功能后才能进行操作的吗?
另外,SPISTE的置位与清零是自动进行还是手动进行?TALK位与其是否有关系?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.