Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
考虑可能时FPUmathtalbes的问题,请问怎么解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
考虑可能时FPUmathtalbes的问题,请问怎么解决?
看看FPUmathtalbes的定义是否正确?
可以参考下面的代码,路径为C:\ti\c2000\C2000Ware_3_01_00_00\libraries\dsp\FPU\c28\examples\common\f2837xd
例程路径为 C:\ti\c2000\C2000Ware_3_01_00_00\libraries\dsp\FPU\c28\examples\fft\2837x_rfft_adc
//#############################################################################
//
// FILE: F2837xD_FPU_RFFT_ADC_lnk.cmd
//
// TITLE: Linker Command File for FPU library examples that run
// on the 2837x platform
//
// This file includes all RAM and FLASH blocks present on the
// 2837x and depending on the active build configuration(RAM or FLASH)
// the appropriate sections will either be loaded into RAM or FLASH
// blocks
//
//#############################################################################
// $TI Release: C28x Floating Point Unit Library V2.03.00.00 $
// $Release Date: Mar 19, 2020 $
// $Copyright: Copyright (C) 2018 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//#############################################################################
// NOTES:
// 1. In addition to this memory linker command file, add the header linker
// command file directly to the project. The header linker command file is
// required to link the peripheral structures to the proper locations within
// the memory map.
//
// The header linker files are found in
// c2000\C2000Ware_X_XX_XX_XX\device_support\f2837x(d/s)\headers\cmd
//
// For BIOS applications add: F2837x(D/S)_Headers_BIOS_cpuX.cmd
// For nonBIOS applications add: F2837x(D/S)_Headers_nonBIOS_cpuX.cmd
//
// 2. On reset all RAMGSx blocks are under the mastership of CPU1. The user
// must configure the appropriate control registers to transfer mastership
// of a RAMGSx block over to CPU2
//
// 3. Memory blocks on F2837x are uniform (ie same physical memory) in both
// PAGE 0 and PAGE 1. That is the same memory region should not be defined
// for both PAGE 0 and PAGE 1. Doing so will result in corruption of program
// and/or data.
//
// Contiguous SARAM memory blocks can be combined if required to create a
// larger memory block.
//
//#############################################################################
// The following definitions will help to align the input buffer.For the complex FFT
// of size N, the input buffer must be aligned to a 4N word boundary. For a real FFT
// of size N, the input buffer must be aligned to a 2N word boundary. The user may define
// the macro either in the linker command file, as shown here, or
// through the project properties under,
// C2000 Linker -> Advanced Options -> Command File Preprocessing -> --define
--define RFFT_ALIGNMENT=1024
#if !defined(RFFT_ALIGNMENT)
#error define RFFT_ALIGNMENT under C2000 Linker -> Advanced Options -> Command File Preprocessing -> --define
#endif
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
#if defined(RAM)
BEGIN : origin = 0x000000, length = 0x000002
#elif defined(FLASH)
BEGIN : origin = 0x080000, length = 0x000002
#endif
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMM1 : origin = 0x000400, length = 0x000400
RAMD0 : origin = 0x00B000, length = 0x000800
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2 : origin = 0x00E000, length = 0x001000
RAMGS3 : origin = 0x00F000, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002
FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS45 : origin = 0x010000, length = 0x002000
RAMGS67 : origin = 0x012000, length = 0x002000
RAMGS89 : origin = 0x014000, length = 0x002000
RAMGS1011 : origin = 0x016000, length = 0x002000
RAMGS12 : origin = 0x018000, length = 0x001000
RAMGS13 : origin = 0x019000, length = 0x001000
RAMGS14 : origin = 0x01A000, length = 0x001000
RAMGS15 : origin = 0x01B000, length = 0x001000
FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
}
SECTIONS
{
codestart : > BEGIN, PAGE = 0
#if defined(RAM)
.TI.ramfunc : > RAMM0, PAGE = 0
.text :>> RAMM1 | RAMD0 | RAMD1 | RAMLS0, PAGE = 0
.cinit : > RAMLS1, PAGE = 0
.pinit : > RAMLS1, PAGE = 0
.switch : > RAMLS1, PAGE = 0
.econst : > RAMLS4, PAGE = 1
#elif defined(FLASH)
.TI.ramfunc : LOAD = FLASHC,
RUN = RAMLS1,
RUN_START(_RamfuncsRunStart),
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
PAGE = 0
.text : > FLASHN, PAGE = 0
.cinit : > FLASHM, PAGE = 0
.pinit : > FLASHM, PAGE = 0
.switch : > FLASHM, PAGE = 0
.econst : > FLASHB, PAGE = 1
#else
#error Add either "RAM" or "FLASH" to C2000 Linker -> Advanced Options -> Command File Preprocessing -> --define
#endif //RAM
/* Test specific sections */
RFFTdata1 : > RAMGS45, PAGE = 1, ALIGN = RFFT_ALIGNMENT
RFFTdata2 : > RAMGS67, PAGE = 1
RFFTdata3 : > RAMGS89, PAGE = 1
RFFTdata4 : > RAMGS1011, PAGE = 1
FPUmathTables : > RAMGS12, PAGE = 1
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.cio : > RAMLS3, PAGE = 1
.sysmem : > RAMLS3, PAGE = 1
.stack : > RAMLS4, PAGE = 1
.ebss : > RAMLS5, PAGE = 1
.esysmem : > RAMLS4, PAGE = 1
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode */
BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS03 : origin = 0x008000, length = 0x003000
/* RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800*/
RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
RAMGS10 : origin = 0x016000, length = 0x001000
RAMGS11 : origin = 0x017000, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
FLASH_API : origin = 0x080004, length = 0x000FFC /* on-chip FLASH */
FLASH_ASM : origin = 0x081000, length = 0x000080 /*commented by ivan @121111*/
FLASH_ENTER : origin = 0x081080, length = 0x000080
FLASH_CODE1 : origin = 0x081100, length = 0x000F00
// FLASHA : origin = 0x080004, length = 0x001FFC /* on-chip Flash */
FLASH_BEGIN : origin = 0x082000, length = 0x000004 /* on-chip Flash */
FLASHB : origin = 0x082004, length = 0x001FFC /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x004000 /* on-chip Flash */
/*FLASHD : origin = 0x086000, length = 0x002000*/ /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x001FD0 /* on-chip Flash */
FLASH_LINK : origin = 0x0BFFD0, length = 0x00002C
FLASH_END : origin = 0x0BFFFC, length = 0x000004 //align(4) lead to this
// FLASHM : origin = 0x0BC000, length = 0x001FD0 /* on-chip Flash */
// FLASH_LINK : origin = 0x0BDFD0, length = 0x00002C
// FLASH_END : origin = 0x0BDFFC, length = 0x000004 //align(4) lead to this
// FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */
BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B000, length = 0x001000
//RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x003000 /*test*/
// RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2 : origin = 0x00F000, length = 0x000C00
RAMGS3 : origin = 0x00FC00, length = 0x000C00
RAMGS4 : origin = 0x010800, length = 0x000C00
RAMGS5 : origin = 0x011400, length = 0x000C00
RAMGS12 : origin = 0x018000, length = 0x002000
// FLASHF : origin = 0x090000, length = 0x002000 /* on-chip Flash */
CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHB PAGE = 0 , ALIGN(4)
.pinit : > FLASHB, PAGE = 0 , ALIGN(4)
.text : >> FLASHE| FLASHG| FLASHH| FLASHI PAGE = 0 , ALIGN(4)
//.text : >> FLASHE| FLASHF| FLASHG| FLASHH| FLASHI PAGE = 0 , ALIGN(4)
// .text : > FLASHB PAGE = 0 , ALIGN(4)
codestart : > BEGIN PAGE = 0 , ALIGN(4)
/*
ramfuncs : LOAD = FLASHD,
RUN = RAMLS03,//RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0 , ALIGN(4)
*/
ramfuncs : LOAD = FLASHC,
RUN = RAMLS03 ,//RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0 , ALIGN(4)
OSStack : > RAMD1 , PAGE = 1
/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
/* .ebss : >> RAMLS5 | RAMGS0 | RAMGS1 PAGE = 1*/
.ebss : > RAMGS0 PAGE = 1
/*.esysmem : > RAMLS5 PAGE = 1*/
.esysmem : > RAMGS2 PAGE = 1
/* Initalized sections go in Flash */
.econst : >> FLASHJ | FLASHK | FLASHL PAGE = 0, ALIGN(4)
.switch : > FLASHM PAGE = 0, ALIGN(4)
FPUmathTables : > RAMGS12, PAGE = 1
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
IAPKEY2 : > FLASH_BEGIN , PAGE = 0, ALIGN(4)
IAPKEY : > FLASH_END , PAGE = 0, ALIGN(4)
IAPLINK : > FLASH_LINK , PAGE = 0, ALIGN(4)
IAPCODE1 : > FLASH_CODE1, PAGE = 0, ALIGN(4)
IAPASM : > FLASH_ASM , PAGE = 0, ALIGN(4)
// IAPCODE2 : > FLASH_CODE2, PAGE = 0, ALIGN(4)
IAPENTER : > FLASH_ENTER, PAGE = 0, ALIGN(4)
IAPAPIDATA : > FLASHL , PAGE = 0, ALIGN(4)
GROUP : LOAD = FLASH_API,
RUN = RAMGS8,
LOAD_START(_RamfuncsIapLoadStart),
LOAD_SIZE(_RamfuncsIapLoadSize),
LOAD_END(_RamfuncsIapLoadEnd),
RUN_START(_RamfuncsIapRunStart),
RUN_SIZE(_RamfuncsIapRunSize),
RUN_END(_RamfuncsIapRunEnd),
PAGE = 0, ALIGN(4)
{
IapConst
ramfuncsIap
}
FLASHTEST2 : > FLASHE , PAGE = 0, ALIGN(4)
FLASHTEST3 : > FLASHG , PAGE = 0, ALIGN(4)
FLASHTEST4 : > FLASHH , PAGE = 0, ALIGN(4)
FLASHTEST5 : > FLASHI , PAGE = 0, ALIGN(4)
FLASHTEST6 : > FLASHJ , PAGE = 0, ALIGN(4)
FLASHTEST7 : > FLASHK , PAGE = 0, ALIGN(4)
FLASHTEST8 : > FLASHM , PAGE = 0, ALIGN(4)
FLASHTEST9 : > FLASHN , PAGE = 0, ALIGN(4)
// FPUmathTables : > RAMGS7, PAGE = 0
// FPUmathTables : > FLASHF, PAGE = 0
FPUmath : LOAD = FLASHF,
RUN = RAMGS7,
//RUN_START(_FPUmathTablesRunStart),
// LOAD_START(_FPUmathTablesLoadStart),
//LOAD_SIZE(_FPUmathTablesLoadSize),
//PAGE = 1
LOAD_START(_FPUmathLoadStart),
LOAD_END(_FPUmathLoadEnd),
RUN_START(_FPUmathRunStart),
PAGE = 0, ALIGN(4)
{
-l rts2800_fpu32_fast_supplement.lib(.text)
}
Filter_RegsFile : > RAMGS0, PAGE = 1
SHARERAMGS0 : > RAMGS2, PAGE = 1
SHARERAMGS1 : > RAMGS3, PAGE = 1
VectorBuff : > RAMGS4, PAGE = 1
DataBuff : > RAMGS5, PAGE = 1
/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}
GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
}