Other Parts Discussed in Thread: C2000WARE
现在使用PWM1和PWM2,PWM1去控制H桥实现逆变,PWM2控制DC-DC BOOST升压电路实现电池升压到直流600V 发现当H桥的SPWM波数据到零点的时候,我需要停止PWM1模块这时会发现会停止PWM2
规格书提示
enabled ePWM modules to the time-base clock (TBCLK). When set, all enabled ePWM module clocks are
started with the first rising edge of TBCLK aligned. For perfectly synchronized TBCLKs, the prescalers for
each ePWM module must be set identically.
The proper procedure for enabling ePWM clocks is as follows:
1. Enable ePWM module clocks in the PCLKCRx register
2. Set TBCLKSYNC= 0
3. Configure ePWM modules
4. Set TBCLKSYNC=1
当我按照Set TBCLKSYNC= 0后发现PWM1和PWM2都会停止运行 这怎么解决 我想单独停止任意一路PWM 谢谢!