采用TI例程can_loopback_interrupts_cpu01 与28377s LAUNCHPAD 开发板测试CAN通信,在运行时总是进入
if(g_bErrFlag)
{
asm(" ESTOP0");
}
程序:
int main(void)
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xS_SysCtrl.c file.
//
InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xS_Gpio.c file and
// illustrates how to set the GPIO to its default state.
//
InitGpio();
// GPIO_SetupPinMux(73, GPIO_MUX_CPU1, 3); // GPIO 73 - XCLKOUT
// GPIO_SetupPinOptions(73, GPIO_OUTPUT, GPIO_PUSHPULL); // SYSCLOCK/8 = 25MHz
GPIO_SetupPinMux(70, GPIO_MUX_CPU1, 1); // GPIO30 - CANRXA
GPIO_SetupPinMux(71, GPIO_MUX_CPU1, 1); // GPIO31 - CANTXA
GPIO_SetupPinOptions(70, GPIO_INPUT, GPIO_ASYNC);
GPIO_SetupPinOptions(71, GPIO_OUTPUT, GPIO_PUSHPULL);
//
// Initialize the CAN controller
//
CANInit(CANA_BASE);
//
// Setup CAN to be clocked off the PLL output clock (500kHz CAN-Clock)
//
CANClkSourceSelect(CANA_BASE, 0);
//
// Set up the bit rate for the CAN bus. This function sets up the CAN
// bus timing for a nominal configuration. You can achieve more control
// over the CAN bus timing by using the function CANBitTimingSet() instead
// of this one, if needed.
// In this example, the CAN bus is set to 500 kHz. In the function below,
// the call to SysCtlClockGet() is used to determine the clock rate that
// is used for clocking the CAN peripheral. This can be replaced with a
// fixed value if you know the value of the system clock, saving the extra
// function call. For some parts, the CAN peripheral is clocked by a fixed
// 8 MHz regardless of the system clock in which case the call to
// SysCtlClockGet() should be replaced with 8000000. Consult the data
// sheet for more information about CAN peripheral clocking.
//
CANBitRateSet(CANA_BASE, 200000000, 500000);
//
// Enable interrupts on the CAN peripheral. This example uses static
// allocation of interrupt handlers which means the name of the handler
// is in the vector table of startup code. If you want to use dynamic
// allocation of the vector table, then you must also call CANIntRegister()
// here.
//外围设备启用中断
CANIntEnable(CANA_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xS_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2837xS_DefaultIsr.c.
// This function is found in F2837xS_PieVect.c.
//
InitPieVectTable();
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
// Register interrupt handler in RAM vector table
//
EALLOW;
PieVectTable.CANA0_INT = CANIntHandler;
EDIS;
//
// Enable the CAN interrupt on the processor (PIE).
//
PieCtrlRegs.PIEIER9.bit.INTx5 = 1;
IER |= 0x0100; // M_INT9
EINT;
//
// Enable test mode and select external loopback
//
HWREG(CANA_BASE + CAN_O_CTL) |= CAN_CTL_TEST;
HWREG(CANA_BASE + CAN_O_TEST) = CAN_TEST_EXL;
//
// Enable the CAN for operation.
//
CANEnable(CANA_BASE);
//
// Enable CAN Global Interrupt line0
//
CANGlobalIntEnable(CANA_BASE, CAN_GLB_INT_CANINT0);
//
// Initialize the message object that will be used for sending CAN
// messages. The message will be 4 bytes that will contain an incrementing
// value. Initially it will be set to 0x12345678.
//
ucTXMsgData[0] = (u32CntTXMsgData>>24) & 0xFF; //右移表示除以2
ucTXMsgData[1] = (u32CntTXMsgData>>16) & 0xFF;
ucTXMsgData[2] = (u32CntTXMsgData>>8) & 0xFF;
ucTXMsgData[3] = (u32CntTXMsgData) & 0xFF;
sTXCANMessage.ui32MsgID = 1; // CAN message ID - use 1
sTXCANMessage.ui32MsgIDMask = 0; // no mask needed for TX
sTXCANMessage.ui32Flags = MSG_OBJ_TX_INT_ENABLE; // enable interrupt on TX
sTXCANMessage.ui32MsgLen = sizeof(ucTXMsgData); // size of message is 8
sTXCANMessage.pucMsgData = ucTXMsgData; // ptr to message content
//
// Initialize the message object that will be used for receiving CAN
// messages.
//
*(unsigned long *)ucRXMsgData = 0;
sRXCANMessage.ui32MsgID = 1; // CAN message ID - use 1
sRXCANMessage.ui32MsgIDMask = 0; // no mask needed for TX
sRXCANMessage.ui32Flags = MSG_OBJ_RX_INT_ENABLE; // enable interrupt on RX
sRXCANMessage.ui32MsgLen = sizeof(ucRXMsgData); // size of message is 8
sRXCANMessage.pucMsgData = ucRXMsgData; // ptr to message content
//
// Setup the message object being used to receive messages
//
CANMessageSet(CANA_BASE, 2, &sRXCANMessage, MSG_OBJ_TYPE_RX);
//
// Send the CAN message using object number 1 (not the same thing as
// CAN ID, which is also 1 in this example). This function will cause
// the message to be transmitted right away.
//
ucTXMsgData[0] = (u32CntTXMsgData>>24) & 0xFF;
ucTXMsgData[1] = (u32CntTXMsgData>>16) & 0xFF;
ucTXMsgData[2] = (u32CntTXMsgData>>8) & 0xFF;
ucTXMsgData[3] = (u32CntTXMsgData) & 0xFF;
//
// Enter loop to send messages. A new message will be sent once per
// second. The 4 bytes of message content will be treated as an unsigned
// long and incremented by one each time.
//
for(;;)
{
//
// Check the error flag to see if errors occurred
//
if(g_bErrFlag)
{
asm(" ESTOP0");
}
if(g_ulTxMsgCount == g_ulRxMsgCount)
{
//
// Transmit Message
//
CANMessageSet(CANA_BASE, 1, &sTXCANMessage, MSG_OBJ_TYPE_TX);
}
else
{
g_bErrFlag = 1;
}
//
// Now wait 1 second before continuing
//
DELAY_US(1000*1000);
//
// Increment the value in the transmitted message data.
//
(*(unsigned long *)ucTXMsgData)++;
}
}
interrupt void
CANIntHandler(void)
{
unsigned long ulStatus;
//
// Read the CAN interrupt status to find the cause of the interrupt
//
ulStatus = CANIntStatus(CANA_BASE, CAN_INT_STS_CAUSE);
//
// If the cause is a controller status interrupt, then get the status
//
if(ulStatus == CAN_INT_INT0ID_STATUS)
{
//
// Read the controller status. This will return a field of status
// error bits that can indicate various errors. Error processing
// is not done in this example for simplicity. Refer to the
// API documentation for details about the error status bits.
// The act of reading this status will clear the interrupt. If the
// CAN peripheral is not connected to a CAN bus with other CAN devices
// present, then errors will occur and will be indicated in the
// controller status.
//
ulStatus = CANStatusGet(CANA_BASE, CAN_STS_CONTROL);
//
//Check to see if an error occurred.
//
if(((ulStatus & ~(CAN_ES_TXOK | CAN_ES_RXOK)) != 7) &&
((ulStatus & ~(CAN_ES_TXOK | CAN_ES_RXOK)) != 0))
{
//
// Set a flag to indicate some errors may have occurred.
//
g_bErrFlag = 1;
}
}
//
// Check if the cause is message object 1, which what we are using for
// sending messages.
//
else if(ulStatus == 1)
{
//
// Getting to this point means that the TX interrupt occurred on
// message object 1, and the message TX is complete. Clear the
// message object interrupt.
//
CANIntClear(CANA_BASE, 1);
//
// Increment a counter to keep track of how many messages have been
// sent. In a real application this could be used to set flags to
// indicate when a message is sent.
//
g_ulTxMsgCount++;
//
// Since the message was sent, clear any error flags.
//
g_bErrFlag = 0;
}
//
// Check if the cause is message object 1, which what we are using for
// receiving messages.
//
else if(ulStatus == 2)
{
//
// Get the received message
//
CANMessageGet(CANA_BASE, 2, &sRXCANMessage, true);
//
// Getting to this point means that the TX interrupt occurred on
// message object 1, and the message TX is complete. Clear the
// message object interrupt.
//
CANIntClear(CANA_BASE, 2);
//
// Increment a counter to keep track of how many messages have been
// sent. In a real application this could be used to set flags to
// indicate when a message is sent.
//
g_ulRxMsgCount++;
//
// Since the message was sent, clear any error flags.
//
g_bErrFlag = 0;
}
//
// Otherwise, something unexpected caused the interrupt. This should
// never happen.
//
else
{
//
// Spurious interrupt handling can go here.
//
}
CANGlobalIntClear(CANA_BASE, CAN_GLB_INT_CANINT0);
PieCtrlRegs.PIEACK.all = PIEACK_GROUP9;
}