Part Number: TMS320F28027
目前项目正在使用PWM控制电源但想做封波处理故用到了错误处理(Trip-zone)模块,我想用软件实现封波即不用外部引脚TZ1 to TZ3实现此功能 看到TZ6可以 但TZ6不知道在程序中怎么实现?
规格书中提到TZ6 TZ6 is connected to EMUSTOP output from the CPU 但我怎么通过编程来实现EMUSTOP ?EMUSTOP 在什么地方有详细介绍?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28027
目前项目正在使用PWM控制电源但想做封波处理故用到了错误处理(Trip-zone)模块,我想用软件实现封波即不用外部引脚TZ1 to TZ3实现此功能 看到TZ6可以 但TZ6不知道在程序中怎么实现?
规格书中提到TZ6 TZ6 is connected to EMUSTOP output from the CPU 但我怎么通过编程来实现EMUSTOP ?EMUSTOP 在什么地方有详细介绍?谢谢!
你好,EMUSTOP是来自CPU的输出信号,用于在CPU停止时关闭PWM,所以应该是不满足你的控制要求的。
有一个寄存器可以用来软件强制TZ事件,你可以看一下TZFRC寄存器。