Part Number: TMS320F280025
Other Parts Discussed in Thread: C2000WARE
你好,问:
1、C:\ti\c2000\C2000Ware_3_04_00_00\device_support\f28002x\examples\timer
280025历程,如定时器和ADC历程,测试连接DSP是成功的,但程序烧录不进去,烧录启动或中途出错是什么原因??帮忙烧录测试下是什么原因?
2、C:\ti\c2000\C2000Ware_3_04_00_00\driverlib\f28002x\examples : 可以正常烧录
出错信息:
C28xx_CPU1: GEL Output:
RAM initialization done
C28xx_CPU1: GEL: Error while executing OnTargetConnect(): identifier not found: ST1
at ST1=(ST1&~(0x0100)) [f280025c.gel:381]
at C28x_Mode() [f280025c.gel:198]
at OnTargetConnect()
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL: Error while executing OnReset(0): identifier not found: XAR0
at XAR0=*((unsigned long *) (0x78000+0x0)) [f280025c.gel:440]
at SetupDCSM() [f280025c.gel:136]
at OnReset(0)
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL: Error while executing OnReset(0): identifier not found: XAR0
at XAR0=*((unsigned long *) (0x78000+0x0)) [f280025c.gel:440]
at SetupDCSM() [f280025c.gel:136]
at OnReset(0)
C28xx_CPU1: GEL: Error while executing OnRestart( 0 ): identifier not found: ST1
at ST1=(ST1&~(0x0100)) [f280025c.gel:381]
at C28x_Mode() [f280025c.gel:164]
at OnRestart(0)
C28xx_CPU1: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x82993: (Error -1066 @ 0x82993) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 9.3.0.00042)
C28xx_CPU1: Breakpoint Manager: Retrying with a AET breakpoint
C28xx_CPU1: Breakpoint Manager: Error enabling this function: Failed to retrieve ID for DCU_SEL.
CCS版本 Version: 10.3.0.00007