Part Number: TMS320F280049C
当把三个ADC模块(ADCA,ADCB,ADCC)的参考电压都配置为内部3.3V时,数值正常
但是当把ADCA与ADCB配置为内部2.5V,ADCC配置为3.3V时,用DAC模块生成1.65V电压时,ADCA与ADCB采样数值正常,但是ADCC采样数值(adcCResult2 )异常。



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049C
当把三个ADC模块(ADCA,ADCB,ADCC)的参考电压都配置为内部3.3V时,数值正常
但是当把ADCA与ADCB配置为内部2.5V,ADCC配置为3.3V时,用DAC模块生成1.65V电压时,ADCA与ADCB采样数值正常,但是ADCC采样数值(adcCResult2 )异常。



用DAC模块生成1.65V电压
这里,你是用DAC生成的1.65V作为参考电压了吗?采样值异常是偏大、偏小还是无规则?
我DAC模块生成的1.65V是用作测试的,如果ADCx的三个模块都是内部参考电压3.3V,那么用这个ADC模块去测量我DAC生产的1.65v,示数正常,但是如果ADCA与ADCB配置为内部2.5V,ADCC配置为3.3V时,ADCC模块采样的数据(adcCResult2 )就会出现异常,我计算后发现这个数据似乎是以5V为基准电压的。因为1365/4096*5V = 1.66V
你好,这个问题只在将参考电压设置为ADCA与ADCB配置为内部2.5V,ADCC配置为3.3V时才出现吗?有测试过其他组合吗?
另外,有没有用外部电压测试一下采样是否正确?
就芯片本身来说,不可能以5V为基准,因为芯片正常工作电压就是3.3V.