This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在调试的时候发现程序开始printf可以正常输出,但后面的printf无输出 请问这什么情况会导致串口刚开始有输出,PWM中断照样运行 就是不知道问题出在哪里 我把代码贴出来,麻烦给予指导,谢谢!
void main(void) { // uint8_t print_cnt1=0,print_cnt2=0; // Step 1. Initialize System Control:b // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2803x_SysCtrl.c InitSysCtrl(); // Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2803x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2803x_DefaultIsr.c. // This function is found in DSP2803x_PieVect.c. InitPieVectTable(); // Copy time critical code and Flash setup code to RAM //实现在RAM中运行代码的搬运,例如使用官方的DELAY_US MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart); InitMyGPIO(); InitKEY();//按键 SCI_Init();//波特率128000bps open_uart_debug(); EALLOW; PieVectTable.EPWM4_INT = &epwm4_isr; EDIS; InitEPWM_AQ_DB(); printf("\r\n\r\n\r\nDSP is Ready");//标准C的printf输出测试,串口调试助手设置波特率128000bps,ASCII格式显示 i=1; printf("\r\n开发板左上角的J4排针(3针),用跳线帽短接靠左的2根针,即为将RG接入到模拟输入口B3"); printf("\r\nPWM频率为19.6KHZ"); //中断配置步骤-----5 PieCtrlRegs.PIEIER3.bit.INTx4 = 1; // Enable the PIE block PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block IER |= M_INT3; EINT; // Enable Global interrupt INTM ERTM;//请参看 使用须知 文件夹下的 分享--ERTM、DRTM 在DSP编程中的作用.pdf printf("\r\nPWM频率为20KHZ 两路PWM"); while(1) { } }
有可能是堆栈空间不够,可以在CCS和cmd文件里面试一下增加一些堆栈空间。
另外可以参考一下这份说明:software-dl.ti.com/.../sdto_cgt_tips_for_using_printf.html