This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2812 中断问题

Other Parts Discussed in Thread: TMS320F28335

请教专家:

flash 起动程序.在仿真时正常运行.在离开仿真后.程序也能正常起动运行.但是不知道什么原因.其中的中断程序运行不正常.请专家给予指教.

  • 1、中断程序是怎么声明和定义的?中断清除有没有?

    2、如何判断是正常启动的?

  • 是这样.运用两个外部中断.XINT1,和XINT2由外部设备触发.当XINT1被触发后.发数据给外部设备.外部设备收到数据,触发XINT2.XINT2处理程序发数据到显示器.现在问题是.在仿真状态.整个过程能完成.在显示器能看到数据.而且不论重复多少次都没问题.但是离开仿真,单独起动运行,能看到显示器开始画面.能操作显示器.但看不到回的数据.显示器的显示和控制,均由F2812通过SPI口进行.现在就是不知道中断有什么问题.或是设置和仿真时要有什么区别.

  • 请问专家:

    TMS320F28335 核电压不足1.8V,只是1.75V  频率150 MHz.对IO口的输出转换.有没影响.经检测.XINT2未被触发.是因为XINT2是由TMS320F28335的IO输出低电平触发的.而F28335的IO电平不按指令转低.所以XINT2未被触发.(但在仿真时能被触发) .请专家指教.

  • QIUPING,

    F28335在150MHz的最低核电压是1.805V,所以你这种情况不排除是这个原因。你可以把主频降低,看是否还存在这个问题。

    另外,你对IO口进行电平切换是使用什么指令?

    Eric