This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: 28388D串口接收无法进入中断的问题

Part Number: TMS320F28388D

我在TMS320F28388D controlCARD进行开发,将sci_ex2_loopback_interrupts.c的例程改为以下,但是无法进入接收中断,请问是为什么?

//###########################################################################
//
// FILE:   sci_ex2_loopback_interrupts.c
//
// TITLE:  SCI Digital Loop Back with Interrupts.
//
//! \addtogroup driver_example_list
//! <h1> SCI Digital Loop Back with Interrupts </h1>
//!
//!  This test uses the internal loop back test mode of the peripheral.
//!  Other then boot mode pin configuration, no other hardware configuration
//!  is required. Both interrupts and the SCI FIFOs are used.
//!
//!  A stream of data is sent and then compared to the received stream.
//!  The SCI-A sent data looks like this: \n
//!  00 01 \n
//!  01 02 \n
//!  02 03 \n
//!  .... \n
//!  FE FF \n
//!  FF 00 \n
//!  etc.. \n
//!  The pattern is repeated forever.
//!
//!  \b Watch \b Variables \n
//!  - \b sDataA - Data being sent
//!  - \b rDataA - Data received
//!  - \b rDataPointA - Keep track of where we are in the data stream.
//!    This is used to check the incoming data
//!
//
//###########################################################################
//
//
// $Copyright: $
//###########################################################################

//
// Included Files
//
#include "driverlib.h"
#include "device.h"

//
// Globals
//

//
// Send data for SCI-A
//
uint16_t sDataA[2];

//
// Received data for SCI-A
//
uint16_t rDataA[2];

//
// Used for checking the received data
//
uint16_t rDataPointA;

//
// Function Prototypes
//
__interrupt void sciaTXFIFOISR(void);
__interrupt void sciaRXFIFOISR(void);
void initSCIAFIFO(void);
void error(void);

//
// Main
//
void main(void)
{
    uint16_t i;

    //
    // Initialize device clock and peripherals
    //
    Device_init();

    //
    // Setup GPIO by disabling pin locks and enabling pullups
    //
    Device_initGPIO();

    //
    // GPIO28 is the SCI Rx pin.
    //
    GPIO_setMasterCore(DEVICE_GPIO_PIN_SCIRXDA, GPIO_CORE_CPU1);
    GPIO_setPinConfig(DEVICE_GPIO_CFG_SCIRXDA);
    GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCIRXDA, GPIO_DIR_MODE_IN);
    GPIO_setPadConfig(DEVICE_GPIO_PIN_SCIRXDA, GPIO_PIN_TYPE_STD);
    GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCIRXDA, GPIO_QUAL_ASYNC);

    //
    // GPIO29 is the SCI Tx pin.
    //
    GPIO_setMasterCore(DEVICE_GPIO_PIN_SCITXDA, GPIO_CORE_CPU1);
    GPIO_setPinConfig(DEVICE_GPIO_CFG_SCITXDA);
    GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCITXDA, GPIO_DIR_MODE_OUT);
    GPIO_setPadConfig(DEVICE_GPIO_PIN_SCITXDA, GPIO_PIN_TYPE_STD);
    GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCITXDA, GPIO_QUAL_ASYNC);

    //
    // Initialize PIE and clear PIE registers. Disables CPU interrupts.
    //
    Interrupt_initModule();

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    //
    Interrupt_initVectorTable();

    //
    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
    //
    Interrupt_register(INT_SCIA_RX, sciaRXFIFOISR);
//    Interrupt_register(INT_SCIA_TX, sciaTXFIFOISR);

    //
    // Initialize the Device Peripherals:
    //
    initSCIAFIFO();

    //
    // Init the send data.  After each transmission this data
    // will be updated for the next transmission
    //
    for(i = 0; i < 2; i++)
    {
        sDataA[i] = i;
    }

    rDataPointA = sDataA[0];

    Interrupt_enable(INT_SCIA_RX);
//    Interrupt_enable(INT_SCIA_TX);

    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);

    //
    // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
    //
    EINT;
    ERTM;

    //
    // IDLE loop. Just sit and loop forever (optional):
    //
    for(;;);
}

//
// error - Function to halt debugger on error
//
void error(void)
{
    asm("     ESTOP0"); // Test failed!! Stop!
    for (;;);
}

//
// sciaTXFIFOISR - SCIA Transmit FIFO ISR
//
__interrupt void sciaTXFIFOISR(void)
{
    uint16_t i;

    SCI_writeCharArray(SCIA_BASE, sDataA, 2);

    //
    // Increment send data for next cycle
    //
    for(i = 0; i < 2; i++)
    {
        sDataA[i] = (sDataA[i] + 1) & 0x00FF;
    }

    SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_TXFF);

    //
    // Issue PIE ACK
    //
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}

//
// sciaRXFIFOISR - SCIA Receive FIFO ISR
//
__interrupt void sciaRXFIFOISR(void)
{
    uint16_t i;

    SCI_readCharArray(SCIA_BASE, rDataA, 2);

    //
    // Check received data
    //
//    for(i = 0; i < 2; i++)
//    {
//        if(rDataA[i] != ((rDataPointA + i) & 0x00FF))
//        {
//            error();
//        }
//    }

    rDataPointA = (rDataPointA + 1) & 0x00FF;

    SCI_clearOverflowStatus(SCIA_BASE);

    SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_RXFF);

    //
    // Issue PIE ack
    //
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}

//
// initSCIAFIFO - Configure SCIA FIFO
//
void initSCIAFIFO()
{
    //
    // 8 char bits, 1 stop bit, no parity. Baud rate is 9600.
    //
    SCI_setConfig(SCIA_BASE, DEVICE_LSPCLK_FREQ, 9600, (SCI_CONFIG_WLEN_8 |
                                                        SCI_CONFIG_STOP_ONE |
                                                        SCI_CONFIG_PAR_NONE));
    SCI_enableModule(SCIA_BASE);
    SCI_disableLoopback(SCIA_BASE);
    SCI_resetChannels(SCIA_BASE);
    SCI_enableFIFO(SCIA_BASE);

    //
    // RX and TX FIFO Interrupts Enabled
    //
    SCI_enableInterrupt(SCIA_BASE, SCI_INT_RXFF);
    SCI_disableInterrupt(SCIA_BASE, SCI_INT_RXERR);

    //
    // The transmit FIFO generates an interrupt when FIFO status
    // bits are less than or equal to 2 out of 16 words
    // The receive FIFO generates an interrupt when FIFO status
    // bits are greater than equal to 2 out of 16 words
    //
    SCI_setFIFOInterruptLevel(SCIA_BASE, SCI_FIFO_TX2, SCI_FIFO_RX2);
    SCI_performSoftwareReset(SCIA_BASE);

//    SCI_resetTxFIFO(SCIA_BASE);
    SCI_resetRxFIFO(SCIA_BASE);
}

//
// End of file
//

  • 烦请标明例程中具体修改的点有哪些。

  • //###########################################################################
    //
    // FILE:   sci_ex2_loopback_interrupts.c
    //
    // TITLE:  SCI Digital Loop Back with Interrupts.
    //
    //! \addtogroup driver_example_list
    //! <h1> SCI Digital Loop Back with Interrupts </h1>
    //!
    //!  This test uses the internal loop back test mode of the peripheral.
    //!  Other then boot mode pin configuration, no other hardware configuration
    //!  is required. Both interrupts and the SCI FIFOs are used.
    //!
    //!  A stream of data is sent and then compared to the received stream.
    //!  The SCI-A sent data looks like this: \n
    //!  00 01 \n
    //!  01 02 \n
    //!  02 03 \n
    //!  .... \n
    //!  FE FF \n
    //!  FF 00 \n
    //!  etc.. \n
    //!  The pattern is repeated forever.
    //!
    //!  \b Watch \b Variables \n
    //!  - \b sDataA - Data being sent
    //!  - \b rDataA - Data received
    //!  - \b rDataPointA - Keep track of where we are in the data stream.
    //!    This is used to check the incoming data
    //!
    //
    //###########################################################################
    //
    //
    // $Copyright: $
    //###########################################################################
    
    //
    // Included Files
    //
    #include "driverlib.h"
    #include "device.h"
    
    //
    // Globals
    //
    
    //
    // Send data for SCI-A
    //
    uint16_t sDataA[2];
    
    //
    // Received data for SCI-A
    //
    uint16_t rDataA[2];
    
    //
    // Used for checking the received data
    //
    uint16_t rDataPointA;
    
    //
    // Function Prototypes
    //
    __interrupt void sciaTXFIFOISR(void);
    __interrupt void sciaRXFIFOISR(void);
    void initSCIAFIFO(void);
    void error(void);
    
    //
    // Main
    //
    void main(void)
    {
        uint16_t i;
    
        //
        // Initialize device clock and peripherals
        //
        Device_init();
    
        //
        // Setup GPIO by disabling pin locks and enabling pullups
        //
        Device_initGPIO();
    
        //
        // GPIO28 is the SCI Rx pin.
        //
        GPIO_setMasterCore(DEVICE_GPIO_PIN_SCIRXDA, GPIO_CORE_CPU1);
        GPIO_setPinConfig(DEVICE_GPIO_CFG_SCIRXDA);
        GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCIRXDA, GPIO_DIR_MODE_IN);
        GPIO_setPadConfig(DEVICE_GPIO_PIN_SCIRXDA, GPIO_PIN_TYPE_STD);
        GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCIRXDA, GPIO_QUAL_ASYNC);
    
        //
        // GPIO29 is the SCI Tx pin.
        //
        GPIO_setMasterCore(DEVICE_GPIO_PIN_SCITXDA, GPIO_CORE_CPU1);
        GPIO_setPinConfig(DEVICE_GPIO_CFG_SCITXDA);
        GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCITXDA, GPIO_DIR_MODE_OUT);
        GPIO_setPadConfig(DEVICE_GPIO_PIN_SCITXDA, GPIO_PIN_TYPE_STD);
        GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCITXDA, GPIO_QUAL_ASYNC);
    
        //
        // Initialize PIE and clear PIE registers. Disables CPU interrupts.
        //
        Interrupt_initModule();
    
        //
        // Initialize the PIE vector table with pointers to the shell Interrupt
        // Service Routines (ISR).
        //
        Interrupt_initVectorTable();
    
        //
        // Interrupts that are used in this example are re-mapped to
        // ISR functions found within this file.
        //
        Interrupt_register(INT_SCIA_RX, sciaRXFIFOISR);
    //注释掉     Interrupt_register(INT_SCIA_TX, sciaTXFIFOISR);  
    
        //
        // Initialize the Device Peripherals:
        //
        initSCIAFIFO();
    
        //
        // Init the send data.  After each transmission this data
        // will be updated for the next transmission
        //
        for(i = 0; i < 2; i++)
        {
            sDataA[i] = i;
        }
    
        rDataPointA = sDataA[0];
    
        Interrupt_enable(INT_SCIA_RX);
    //注释掉    Interrupt_enable(INT_SCIA_TX);
    
        Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
    
        //
        // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
        //
        EINT;
        ERTM;
    
        //
        // IDLE loop. Just sit and loop forever (optional):
        //
        for(;;);
    }
    
    //
    // error - Function to halt debugger on error
    //
    void error(void)
    {
        asm("     ESTOP0"); // Test failed!! Stop!
        for (;;);
    }
    
    //
    // sciaTXFIFOISR - SCIA Transmit FIFO ISR
    //
    __interrupt void sciaTXFIFOISR(void)
    {
        uint16_t i;
    
        SCI_writeCharArray(SCIA_BASE, sDataA, 2);
    
        //
        // Increment send data for next cycle
        //
        for(i = 0; i < 2; i++)
        {
            sDataA[i] = (sDataA[i] + 1) & 0x00FF;
        }
    
        SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_TXFF);
    
        //
        // Issue PIE ACK
        //
        Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
    }
    
    //
    // sciaRXFIFOISR - SCIA Receive FIFO ISR
    //
    __interrupt void sciaRXFIFOISR(void)
    {
        uint16_t i;
    
        SCI_readCharArray(SCIA_BASE, rDataA, 2);
    
        //
        // Check received data
        //
    //    for(i = 0; i < 2; i++)
    //    {
    //        if(rDataA[i] != ((rDataPointA + i) & 0x00FF))
    //        {
    //            error();
    //        }
    //    }
    
        rDataPointA = (rDataPointA + 1) & 0x00FF;
    
        SCI_clearOverflowStatus(SCIA_BASE);
    
        SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_RXFF);
    
        //
        // Issue PIE ack
        //
        Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
    }
    
    //
    // initSCIAFIFO - Configure SCIA FIFO
    //
    void initSCIAFIFO()
    {
        //
        // 8 char bits, 1 stop bit, no parity. Baud rate is 9600.
        //
        SCI_setConfig(SCIA_BASE, DEVICE_LSPCLK_FREQ, 9600, (SCI_CONFIG_WLEN_8 |
                                                            SCI_CONFIG_STOP_ONE |
                                                            SCI_CONFIG_PAR_NONE));
        SCI_enableModule(SCIA_BASE);
        SCI_disableLoopback(SCIA_BASE); //将enable 改为 disable 
        SCI_resetChannels(SCIA_BASE);
        SCI_enableFIFO(SCIA_BASE);
    
        //
        // RX and TX FIFO Interrupts Enabled
        //
        SCI_enableInterrupt(SCIA_BASE, SCI_INT_RXFF);       //去掉| SCI_INT_TXFF
        SCI_disableInterrupt(SCIA_BASE, SCI_INT_RXERR);
    
        //
        // The transmit FIFO generates an interrupt when FIFO status
        // bits are less than or equal to 2 out of 16 words
        // The receive FIFO generates an interrupt when FIFO status
        // bits are greater than equal to 2 out of 16 words
        //
        SCI_setFIFOInterruptLevel(SCIA_BASE, SCI_FIFO_TX2, SCI_FIFO_RX2);
        SCI_performSoftwareReset(SCIA_BASE);
    
    //注释掉    SCI_resetTxFIFO(SCIA_BASE);
        SCI_resetRxFIFO(SCIA_BASE);
    }
    
    //
    // End of file
    //

    好的好的,具体如上,主要是将Loopback功能取消了,然后注释掉了发送中断相关的指令,具体已在代码中中文备注

  • 您好,问题解决了,是我在硬件上没有将S1置为ON的状态

  • 好的,感谢反馈