This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28054M: 想使用flash模拟eeprom功能,存取一个字节的数据

Part Number: TMS320F28054M
Other Parts Discussed in Thread: C2000WARE

参考的《第2代C2000实时MCU的EEPROM 模拟》和《Flash2805x_API_Quickstart》两个手册和c2000\C2000Ware_3_04_00_00\libraries\flash_api\f2805的例程,目前遇到的问题是:

1:2805x_BootROM_API_TABLE_Symbols.lib 和Flash2805x_API_V100.lib,这两个用哪个,对应的cmd文件该如何配置,

2:#pragma DATA_SECTION(Flash_CPUScaleFactor, "FlashScalingVar");
#pragma DATA_SECTION(Flash_CallbackPtr, "FlashCallbackVar");
void (*Flash_CallbackPtr) (void);

Uint32 Flash_CPUScaleFactor;

"FlashCallbackVar"和"FlashScalingVar"的内存空间应该写在现有的cmd文件中,还是添加F2805x_Headers_nonBIOS,如果添加,又要怎么修改

3:

Step 6: Copy the Flash API functions to Internal SARAM,这一步该怎么做,

  • 其实我感觉你问的问题基本在《Flash2805x_API_Quickstart》上都有说明

    1、在20. Files included with the API中有说明

    2、这两个是定义在cmd文件中的,具体可以参考一下例程里面的定义方法:C:\ti\c2000\C2000Ware_4_00_00_00\libraries\flash_api\f2805x

    3、这步就是将flashAPI函数从flash搬移到ram运行,就是调用memcopy函数,这里文档上的说明有什么不理解的吗?

  • 1.“20. Files included with the API”看的不明白,这里我可以再去看看

    2.