This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
currently we plan to use TMS3120F28388S with ethercat function, but cannot get DP83822 chip, want to change it into LAN8720, have one question, is it ok for ethercat? have any porting example code for us?
抱歉对这款产品不了解,也没有找到C2000芯片和这款ethercat芯片一起使用的范例。
你可以看一下F28388S的Ethercat协议:
The Ethernet module enables a host to transmit and receive data over the Ethernet in compliance with IEEE
802.3-2015. The Ethernet module contains the following characteristics:
• IEEE 802.3-2015 for Ethernet MAC, Media Independent Interface (MII)
• IEEE 1588-2008 for precision networked clock synchronization
• IEEE 802.3az-2010 for Energy Efficient Ethernet (EEE)
• Reduced Media Independent Interface (RMII) specification version 1.2 from RMII consortium
• Reverse Media Independent Interface (RevMII)