Part Number: TMS320F28379D
预计用ePWM输出电压可调的负电压,但输出的高电平为正3.3v,请问如何将之变为负的?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,由芯片输出的PWM信号都是0~3.3V的数字信号,没有负值电压输出。
如果要获得负值电压的话一般都要通过后端电路将PWM信号逆变为交流信号等等方式才会获得负的电压。
你好,DAC也不可以,只能通过外接运放实现负电压。
ADC模块只能接受很小的负电压,但也不能读取负值电压,ADC的输入电压范围是–0.3~4.6V,转换的范围是0~VREFHI