This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
FLASH编程正常,擦除总是报错,每次擦除会进入非法中断:Interrupt_illegalOperationHandler,然后就卡死了。
核心代码如下:
const Uint32 flashSectorStart[14] = { 0x080000, 0x082000, 0x084000, 0x086000, 0x088000, 0x090000, 0x098000, 0x0A0000, 0x0A8000, 0x0B0000, 0x0B8000, 0x0BA000, 0x0BC000, 0x0BE000 }; const Uint32 flashSectorSize[14] = { 0x2000, 0x2000, 0x2000, 0x2000, 0x8000, 0x8000, 0x8000, 0x8000, 0x8000, 0x8000, 0x2000, 0x2000, 0x2000, 0x2000, }; // sector = a-n #pragma CODE_SECTION(eraseFlashSector,".TI.ramfunc"); Uint32 eraseFlashSector(Uint16 sector) { Uint32 addr = 0; Fapi_StatusType oReturnCheck; Fapi_FlashStatusType oFlashStatus; if(sector < 'a' || sector > 'n') { return 0; } addr = flashSectorStart[sector - 'a']; #if 1 DINT; EALLOW; oReturnCheck = Fapi_issueAsyncCommandWithAddress(Fapi_EraseSector, (uint32*)addr); while (Fapi_checkFsmForReady() != Fapi_Status_FsmReady){} if(oReturnCheck != Fapi_Status_Success) { printx("oReturnCheck = 0x__\r\n", oReturnCheck); } oFlashStatus = Fapi_getFsmStatus(); if(oFlashStatus != 0) { printx("oFlashStatus = 0x__\r\n", oFlashStatus); } EDIS; EINT; #endif return addr; }
PLL输出120M,使用内部INTOSC2和外部16M晶振都试过,现象一样。
cmd文件中通过-lF021_API_F2837xD_FPU32.lib(.text)将F021库放入SRAM,并且通过map文件检查,相关代码都在SRAM中。
F021库版本为1.54,F28075和F2837x使用相同的F021固件库没错吧?是否有需要特别注意的地方?
自己搞定了,公布答案:在等待扇区擦除完成的while循环中,一定要踢狗。官方例程
C2000Ware_4_00_00_00\device_support\f2807x\examples\cpu1\flash_programming\cpu01\flash_programming_cpu01.c里面等待擦除完毕是这样写的:
while (Fapi_checkFsmForReady() != Fapi_Status_FsmReady){}
没有踢狗,因为2k扇区擦除时间典型值为35ms,而默认看门狗配置大约13ms就会复位,所以一定要踢狗。正确代码是这样:
while (Fapi_checkFsmForReady() != Fapi_Status_FsmReady){SysCtl_serviceWatchdog();}
这是一个非常隐蔽的坑,我查了一整天才查出来,希望TI能修改一下例程,不要给用户挖这种高级而又隐蔽的坑。