This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: Test connection成功,connect target失败

Part Number: TMS320F28377D


ccs10, 28377d,XDS200仿真器,Test connection成功,connect target失败,报错信息如下:

C28xx_CPU1: Trouble Reading Register ST1: (Error -1041 @ 0x5F453) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.2.0.00002)
C28xx_CPU1: GEL: Error while executing OnTargetConnect(): Target failed to read register ST1
at (ST1&~(0x0100)) [f28377d_cpu1.gel:312]
at C28x_Mode() [f28377d_cpu1.gel:88]
at OnTargetConnect()
C28xx_CPU1: Error initializing flash programming: Interface returned from dll, but flash is not available on this device.
C28xx_CPU1: Breakpoint Manager: Error enabling this function: ACU_SEL Register write failed
C28xx_CPU1: Error: (Error -1135 @ 0x822A7) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.2.0.00002)
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging

断电,拔掉仿真器重连几次都这样