Part Number: TMS320F28069
我今天配置了一个XDS100 V1 JTAG 准备给TI 28069 去灌程序,TestConnection 都是OK 的,但是启动Debug 的时候,报告:
Error connecting to the target:
(Error -1015 @ 0x0)
Device is not responding to the request. Device may be locked, or the debug probe connection may be unreliable. Unlock the device if possible (e.g. use wait in reset mode, and power-cycle the board). If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 6.0.407.3)
有没有人遇到过啊?
前面TestConnection 是OK的: