This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: CLA定义里的warning

Part Number: TMS320F280039C


各位大神好:

我在新建的280039工程里编译了下,结果以下语句报warning:

CLA_mapTaskVector(CLA1_BASE, CLA_MVECT_1, (uint16_t)&Cla1Task1);
CLA_mapTaskVector(CLA1_BASE, CLA_MVECT_2, (uint16_t)&Cla1Task2);
CLA_mapTaskVector(CLA1_BASE, CLA_MVECT_3, (uint16_t)&Cla1Task3);
CLA_mapTaskVector(CLA1_BASE, CLA_MVECT_4, (uint16_t)&Cla1Task4);
CLA_mapTaskVector(CLA1_BASE, CLA_MVECT_5, (uint16_t)&Cla1Task5);
CLA_mapTaskVector(CLA1_BASE, CLA_MVECT_6, (uint16_t)&Cla1Task6);
CLA_mapTaskVector(CLA1_BASE, CLA_MVECT_7, (uint16_t)&Cla1Task7);

CLA_mapBackgroundTaskVector(CLA1_BASE,  (uint16_t)&Cla1BackgroundTask);

CCS的描述是:
#770-D conversion from pointer to smaller integer 

但是之前的280049的程序,同样的语句没有报错,很疑惑。