This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: 在线可仿真运行,离线无法运行的问题

Part Number: TMS320F28388D


实验一:
1、程序内容
6轴ethercat从站代码+6轴电机驱动代码
2、问题描述
1)6轴ethercat从站代码+5轴电机驱动代码,可以在线flash仿真运行,重新断电再上电后,可以离线运行
2)6轴ethercat从站代码+6轴电机驱动代码,可以在线flash仿真运行,重新断电再上电后,无法离线运行
3、备注:
1)以上实验,ethercat从站代码和电机驱动代码所定义的轴数通过宏定义完成
2)以上实验,所使用的cmd文件为同一个文件,在附件中名称为:2838x_FLASH_lnk_ecat_cpu1.cmd
3)6轴ethercat从站代码+5轴电机驱动代码的map为附件中6e5m.map;6轴ethercat从站代码+6轴电机驱动代码的map为附件中6e6m.map;
4)开发人员已经尝试过很多cmd配置组合,依然无法解决6轴ethercat从站代码+6轴电机驱动代码离线无法运行问题。
5)开发人员尝试测试过28388D的RAM,发现在cmd配置足够空间的bss段的情况下,程序能够申明和定义的全局float数组大小不能超过3000,否则程序依然无法离线运行。tms320f28388d问题分析.zip