This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教个问题。型号TMS320F28379D,定时器中断控制SPI发送正弦波速度,中断频率提高到80k,正弦波频率就无法再提高是为什么?16位的ADC,无论是软件触发连续采样,还是通过EPWM触发在ADC中断中采样,最终数组导出的采样结果来看,采样频率只有80k,远没有达到1MHz,请求解答。
你好,采样频率的话不仅受触发频率影响,还受比如其他中断侵占ADC中断时间、采样窗(S/H)大小等等影响。
你有没有用例程测试过?例程的话只包含采样程序,测试起来会干净很多。修改宏定义就可以切换16位采样模式了:
C:\ti\c2000\C2000Ware_4_00_00_00\driverlib\f2837xd\examples\cpu1\adc
1.基于TI的28379控制卡做的电路板,SPI发送正弦波,无其他中断侵占ADC中断事件问题,采集窗口是默认值,在主程序中软件触发连续采样,得到的采样频率还是很低。
2.由于电源电压问题,用的其他28379学习板去采集信号发生器1KHz正弦波,用例程采集一个周期100个点,还是不高。
3.TI的手册16位ADC是可以达到1.1M的采样频率,是否其他方式直接查看ADC采样频率,有哪些可能的办法提高ADC采样频率?
你好,不知道是不是程序设置问题,但是100k的采样频率确实不算高了,F28379D应该完全可以达到的。
你可以参考一下这个帖子中的回复,看看是否能有所帮助:e2e.ti.com/.../tms320f28377s-maximum-adc-sampling-rate