This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
C28xx_CPU1: Trouble Reading Register PC: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.2.0.00002)
C28xx_CPU1: Trouble Reading Register PC: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.2.0.00002)
C28xx_CPU1: Trouble Reading Register PC: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.2.0.00002)
使用28377D程序可以load进RAM但是无法运行?请问是什么原因呢?
你好,是自己制作的板子?之前能正常使用吗?
另外,仿真器连接测试是succeed的?芯片的boot引脚设置正确吗?
之前的问题解决了,现在出现了新的问题。
现在是插上外设就会报错,错误如下:
C28xx_CPU1:错误:(错误-1044@0x0)调试探测报告了一个错误。确认调试探测配置和连接,重置调试探测,然后重试该操作。(仿真包9.2.0.00002)
C28xx_CPU1:错误:(错误-1135@0x864C)调试探针报告了一个错误。确认调试探测配置和连接,重置调试探测,然后重试该操作。(仿真包9.2.0.00002)
C28xx_CPU1:尝试20次后无法确定目标状态
C28xx_CPU1:未能在断开连接之前从目标中删除调试状态。程序内存中可能仍有断点操作码。建议在连接和重新加载程序之前重置模拟器,然后再继续调试
请问是不是哪里配置的不对?
DSP没有外设的时候是可以跑起来的,但是插上外设就报错。请问如何解决呢?
这样的话我觉得这个问题应该跟你插上的外设有关联啊,具体是什么外设呢?