因为目前做的UPS的逆变的值的AD采样值固定,故把200个数组存在M24C02 ,现在有个疑问,在PWM中断(中断频率为20K),并且考虑到中断从TBPRD-25处发生就相当于每次中断的有效时间只有20K的一半,故用TMS320F28027自身的IIC在中断中一次读取5个字节数据是否会造成超过中断时间?
此外官方有没有M2402的例程?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
因为目前做的UPS的逆变的值的AD采样值固定,故把200个数组存在M24C02 ,现在有个疑问,在PWM中断(中断频率为20K),并且考虑到中断从TBPRD-25处发生就相当于每次中断的有效时间只有20K的一半,故用TMS320F28027自身的IIC在中断中一次读取5个字节数据是否会造成超过中断时间?
此外官方有没有M2402的例程?谢谢!
不好意思,问题描述的没看懂。
是不是说,在40KHz的PWM频率情况下,能否在一个PWM中断中完成I2C读取5个字节数据?有什么需要补充的地方吗?
官方只提供了一个I2C访问外部eeprom的例程。
你好,我认为是可以的。I2C的通讯速率最高可以达到400kbps,而且还具有16字节深度的硬件FIFO。