28377D芯片中的GPIO84和GPIO72都要通过电阻上拉,那如果需要使用以太网功能时,是不是GPIO72不能作为EM1D12呀?此时是不是以太网需要使用EM2相关引脚呀?如果把GPIO72作为EM1D12时,不能把程序加载到Flash,只能通过上拉GPIO72才能加载,所以是不是以太网需要寻找对应的位置(如GPIO56/EM2D12)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
28377D芯片中的GPIO84和GPIO72都要通过电阻上拉,那如果需要使用以太网功能时,是不是GPIO72不能作为EM1D12呀?此时是不是以太网需要使用EM2相关引脚呀?如果把GPIO72作为EM1D12时,不能把程序加载到Flash,只能通过上拉GPIO72才能加载,所以是不是以太网需要寻找对应的位置(如GPIO56/EM2D12)?
不是,GPIO引脚的功能可以正常使用。boot引脚只需要在上电的时候保持boot需要的电位就可以,上电完成后就可以释放。或者你也可以在GPIO引脚上做一个弱上/下拉,这样即使上电完成也不需要做硬件上的处理。