This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 SPI口速率

    目前碰到一个问题,28335的SPI口速率上不去!具体情况是:使用28335与SPI口ADC连接时,由于使用中对于SPI口速率要求较高,故将SPI口速率配置为18.75M(内部倍频至150M运行,SPI采用GPIO54-57),但看波形明显是不满足的,后看资料说与SPI口所用GPIO的I/O buffer的速率有关,查遍手头能查资料,未找到有关配置的说明。现在SPI口配置为2M多,波形勉强算可以,但这样无法满足我的使用要求。想请教如何才能提升SPI口速率?

  • 芯片的SPI时钟由LSPCLK提供,把LSPCLK设置到最大75MHZ。然后SPICLK接收速率最高12.5MHZ,把SPIBRR设为5.这时候SPI的接收速度最快。另外也建议看一下ADC芯片所支持的SPI最高CLK速度。

    更详细的信息可以参考datasheet的Electrical Specifications章节。

     

  • 感谢回复,我已经看到此设置了,但问题是当我设置到比较高的速度时,SCLK出来的波形是非常差的,类似于三角波,而且峰值到不了3V,低电平到不了0V,而在SPRUEU3A.pdf中看到这样一句话,“The maximum baud rate that can be employed is limited by the maximum speed of the I/O buffers used on the SPI pins.“,所以觉得会不会是I/O口的速度影响了SPI口速率,但这样的话,芯片设计岂不是有矛盾?

    还是怀疑自己的设置有问题,但不知道问题出在哪里,还请再帮忙详细看看具体应当如何设置,或有相应的例程,不胜感谢!

  • 例程可以直接使用TI例程包中的,spi_loopback_interrupts例程。我试了一下,在不连接外部设备的时候,SPICLK的12.5MHZ波形很好。

    “The maximum baud rate that can be employed is limited by the maximum speed of the I/O buffers used on the SPI pins.“

    这句话我的理解是,SPI最大速率受SPI引脚所在连接的外部系统的buffers 影响。

  • 好的,这样我心里就有底了,我再试试看,感谢Forrest TX!