This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: 寄存器ADCSOC0CTL的CHSEL如果要选择C3,D5这样的引脚,CHSEL该如何赋值, 它的值如下,好像就只能A0~A7,B0~B7

Part Number: TMS320F28379D


Single-ended Signaling Mode (SIGNALMODE = 0):
0h ADCIN0
1h ADCIN1
2h ADCIN2
3h ADCIN3
4h ADCIN4
5h ADCIN5
6h ADCIN6
7h ADCIN7
8h ADCIN8
9h ADCIN9
Ah ADCIN10
Bh ADCIN11
Ch ADCIN12
Dh ADCIN13
Eh ADCIN14
Fh ADCIN15